This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-software:build-the-zynq-boot-image [14 Feb 2018 16:11] – Michael Hennerich | resources:tools-software:linux-software:build-the-zynq-boot-image [10 Jan 2022 09:20] – [Usage] Stefan-Robert Raus | ||
---|---|---|---|
Line 34: | Line 34: | ||
< | < | ||
- | usage: build_boot_bin.sh system_top.hdf u-boot.elf [output-archive] | + | usage: build_boot_bin.sh system_top.xsa u-boot.elf [output-archive] |
</ | </ | ||
- | * Path to '' | + | * Path to '' |
* An optionally 3rd '' | * An optionally 3rd '' | ||
* Build output is located in a local directory named: output_boot_bin. | * Build output is located in a local directory named: output_boot_bin. | ||
- | * This script requires Xilinx | + | * This script requires Xilinx |
* A simple way is to source vivado settings[32|64].sh: | * A simple way is to source vivado settings[32|64].sh: | ||
< | < | ||
- | $ source / | + | $ source / |
</ | </ | ||
+ | * When using **cygwin**, you can add the following in the ~/.bashrc configuration file: | ||
+ | |||
+ | < | ||
+ | export PATH=$PATH:/ | ||
+ | export PATH=$PATH:/ | ||
+ | </ | ||
+ | There is also a version of script that works in Windows Powershell: [[ https:// | ||
< | < |