This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-software:adrv9009_plugin [04 Jun 2018 17:17] – [Transmit Chain] Michael Hennerich | resources:tools-software:linux-software:adrv9009_plugin [22 Jul 2020 14:51] (current) – [ADRV9009 Plugin Description] Michael Hennerich | ||
---|---|---|---|
Line 4: | Line 4: | ||
If you want to go play with ''/ | If you want to go play with ''/ | ||
+ | |||
+ | <note tip> | ||
+ | This plugin supports multiple device instantiations. Typically used in a multichip design, where all devices and links are being synchronized. | ||
+ | In order to support this mode, all IIO devices need unique names. | ||
+ | Such as: | ||
+ | < | ||
+ | adrv9009-phy-d | ||
+ | adrv9009-phy-c | ||
+ | adrv9009-phy-b | ||
+ | adrv9009-phy-a [JESD204 FSM Top Device] | ||
+ | </ | ||
+ | or: | ||
+ | < | ||
+ | adrv9009-phy-3 | ||
+ | adrv9009-phy-2 | ||
+ | adrv9009-phy-1 | ||
+ | adrv9009-phy-0 [JESD204 FSM Top Device] | ||
+ | </ | ||
+ | |||
+ | When used with the JESD204 finite state machine framework. The Top Device needs to be suffixed with a letter or numeral smaller than the slave devices. | ||
+ | (a < b < c … or 0 < 1 < 2 …) | ||
+ | </ | ||
+ | |||
If you think the device has a setting that isn't managed by this tab, check out the [[adrv9009_advanced_plugin|ADRV9009 Advanced Plugin]] for the IIO Oscilloscope. | If you think the device has a setting that isn't managed by this tab, check out the [[adrv9009_advanced_plugin|ADRV9009 Advanced Plugin]] for the IIO Oscilloscope. | ||
Line 66: | Line 89: | ||
* **Tracking** [[: | * **Tracking** [[: | ||
* **Quadrature** | * **Quadrature** | ||
- | | + | |
==== FPGA Settings ==== | ==== FPGA Settings ==== | ||
=== Transmit/ | === Transmit/ |