This is an old revision of the document!
Function | File |
---|---|
driver | sound/soc/codecs/ssm2518.c |
include | sound/soc/codecs/ssm2518.h |
For compile time configuration, it’s common Linux practice to keep board- and application-specific configuration out of the main driver file, instead putting it into the board support file.
For devices on custom boards, as typical of embedded and SoC-(system-on-chip) based hardware, Linux uses platform_data to point to board-specific structures describing devices and how they are connected to the SoC. This can include available ports, chip variants, preferred modes, default initialization, additional pin roles, and so on. This shrinks the board-support packages (BSPs) and minimizes board and application specific #ifdefs in drivers.
Unlike PCI or USB devices, I2C devices are not enumerated at the hardware level. Instead, the software must know which devices are connected on each I2C bus segment, and what address these devices are using. For this reason, the kernel code must instantiate I2C devices explicitly. There are different ways to achieve this, depending on the context and requirements. However the most common method is to declare the I2C devices by bus number.
This method is appropriate when the I2C bus is a system bus, as in many embedded systems, wherein each I2C bus has a number which is known in advance. It is thus possible to pre-declare the I2C devices that inhabit this bus. This is done with an array of struct i2c_board_info, which is registered by calling i2c_register_board_info().
So, to enable such a driver one need only edit the board support file by adding an appropriate entry to i2c_board_info.
For more information see: Documentation/i2c/instantiating-devices.rst
The I2C address of the SSM2518 depends on the setting of the ADDR pin
ADDR | I2C Address |
---|---|
0 | 0x34 |
1 | 0x36 |
static struct i2c_board_info __initdata bfin_i2c_board_info[] = { [--snip--] { I2C_BOARD_INFO("ssm2518", 0x34), }, [--snip--] }
static int __init stamp_init(void) { [--snip--] i2c_register_board_info(0, bfin_i2c_board_info, ARRAY_SIZE(bfin_i2c_board_info)); [--snip--] return 0; } arch_initcall(board_init);
i2s: i2c@41600000 { compatible = "...; ... #size-cells = <0>; #address-cells = <1>; ssm2518: ssm2518@34 { compatible = "adi,ssm2518"; reg = <0x34>; gpios = <&gpio 5 0>; }; };
Name | Description |
---|---|
OUTL | Output for Left Channel |
OUTR | Output for Right Channel |
Name | Description |
---|---|
Playback De-emphasis Switch | Enable/Disable de-emphasis |
Master Playback Volume | DAC Volume Control |
Master Playback Switch | Unmutes/Mutes the DAC output |
Amp Low Power Mode Switch | Enables/Disables the lower power mode of the Amplifier |
DAC Low Power Mode Switch | Enables/Disables the lower power mode of the DAC |
DRC Switch | Enable/Disable Dynamic Range Control |
DRC Limiter Switch | Enable/Disable the DRC Limiter function |
DRC Compressor Switch | Enable/Disable the DRC Compressor function |
DRC Expander Switch | Enable/Disable the DRC Expander function |
DRC Noise Gate Switch | Enable/Disable the DRC Noise Gate function |
DRC Limiter Threshold Volume | DRC Limiter Threshold Setting. Relative to input |
DRC Compressor Lower Threshold Volume | DRC Compressor Lower Threshold Setting. Relative to input |
DRC Expander Upper Threshold Volume | DRC Expander Upper Threshold Setting. Relative to input |
DRC Noise Gate Threshold Volume | DRC Noise Gate Threshold Setting. Relative to input |
DRC Upper Output Threshold Volume | DRC Limiter Threshold Setting. Relative to input |
DRC Lower Output Threshold Volume | DRC Minimum Output Signal Amplitude Setting. This is the minimum output level produced by the DRC and is used to indicate the expander lower threshold, or output signal level when the input rises beyond the noise gate threshold |
DRC Post Volume | Post-DRC Gain Adjust Setting. This can be used to add additional gain after the DRC function to compensate for the overall reduction of system gain due to the DRC |
DRC Peak Detector Attack Time | DRC Peak Detector Attack Time |
DRC Peak Detector Release Time | DRC Peak Detector Release Time |
DRC Attack Time | DRC Attack Time. Used to smooth the gain curve at the thresholds (knees) of each DRC function |
DRC Decay Time | DRC Decay Time. Used to smooth the gain curve at the thresholds (knees) of each DRC function |
DRC Hold Time | DRC Normal Operation Hold Time. Used to prevent the gain curve calculation from increasing too quickly |
DRC Noise Gate Hold Time | |
DRC RMS Averaging Time | DRC RMS Detector Averaging Time. This is the averaging time for the rms level that is compared to the DRC thresholds |
The codec driver registers one DAI named “ssm2518-hifi”.
Name | Supported by driver | Description |
---|---|---|
SND_SOC_DAIFMT_I2S | yes | I2S Justified mode |
SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode |
SND_SOC_DAIFMT_LEFT_J | yes | Left Justified mode |
SND_SOC_DAIFMT_DSP_A | yes | data MSB after FRM LRC |
SND_SOC_DAIFMT_DSP_B | yes | data MSB during FRM LRC |
SND_SOC_DAIFMT_AC97 | no | AC97 mode |
SND_SOC_DAIFMT_PDM | no | Pulse density modulation |
SND_SOC_DAIFMT_NB_NF | yes | Normal bit- and frameclock |
SND_SOC_DAIFMT_NB_IF | yes | Normal bitclock, inverted frameclock |
SND_SOC_DAIFMT_IB_NF | yes | Inverted frameclock, normal bitclock |
SND_SOC_DAIFMT_IB_IF | yes | Inverted bit- and frameclock |
SND_SOC_DAIFMT_CBM_CFM | no | Codec bit- and frameclock master |
SND_SOC_DAIFMT_CBS_CFM | no | Codec bitclock slave, frameclock master |
SND_SOC_DAIFMT_CBM_CFS | no | Codec bitclock master, frameclock slave |
SND_SOC_DAIFMT_CBS_CFS | yes | Codec bit- and frameclock slave |
The CODECs system clock can be configured for various input rates. When configuring the codec system clock use SSM2518_SYSCLK for the clock id.
The following list contains the supported system clock rates and their resulting sample-rates.
SYSCLK | Supported sample-rates |
---|---|
2048000, 4096000, 8192000, 8192000, 3200000, 6400000, 12800000 | 8kHz, 16kHz, 32kHz |
2822000, 5644800, 11289600, 16934400, 22579200, 33868800, 4410000, 8820000, 17640000 | 11.025kHz, 22.05kHz, 44.1kHz |
3072000, 6144000, 38864000, 4800000, 9600000, 19200000 | 12kHz, 24kHz, 48kHz, 96kHz |
12288000, 16384000, 24576000 | 8kHz, 12kHz, 16kHz, 24kHz, 32kHz, 48kHz, 96kHz |
To configure the devices sysclk the snd_soc_codec_set_sysclk()
function can be used. It needs to be called at least once before playback starts. The clk_id
parameter must always be SSM2518_SYSCLK
and the dir
parameter must always be SND_SOC_CLOCK_IN
. The freq
can be set to any of the frequencies above. The system clock can either be taken from the external MCLK or the BCLK. In case the system clock is taken from the BCLK the BCLK needs to be applied to the MCLK pin and the BLCK can be left unconnected. To use the MCLK as the system clock source the source
parameter should to be set to SSM2518_SYSCLK_SRC_MCLK
, to use the BCLK it should be set to SSM2518_SYSCLK_SRC_BCLK
#define SSM2518_SYSCLK 0 enum ssm2518_sysclk_src { SSM2518_SYSCLK_SRC_MCLK = 0, SSM2518_SYSCLK_SRC_BCLK = 1, };
If you want to use the SSM2518 in TDM mode you can configure it using snd_soc_dai_set_tdm_slot() from you ASoC board driver.
The following restrictions apply to the parameters of snd_soc_dai_set_tdm_slot().
Example:
static int ssm2518_link_init(struct snd_soc_pcm_runtime *rtd) { int ret; ret = snd_soc_dai_set_tdm_slot(rtd->codec_dai, 0x0c, 0x00, 8, 32); if (ret < 0) return ret; return 0; } static struct snd_soc_dai_link ssm2518_dai_link = { ..., .init = ssm2518_link_init, };
#include "../codecs/ssm2518.h" static int pmod_amp3_init(struct snd_soc_pcm_runtime *rtd) { return snd_soc_codec_set_sysclk(rtd->codec, SSM2518_SYSCLK, SSM2518_SYSCLK_SRC_MCLK, 12288000, SND_SOC_CLOCK_IN); } static const struct snd_soc_dapm_widget pmod_amp3_widgets[] = { SND_SOC_DAPM_SPK("Speaker Out", NULL), }; static const struct snd_soc_dapm_route pmod_amp3_routes[] = { { "Speaker Out", NULL, "OUTL" }, { "Speaker Out", NULL, "OUTR" }, }; static struct snd_soc_dai_link pmod_amp3_dai_link = { .name = "ssm2518", .stream_name = "ssm2518", .codec_dai_name = "ssm2518-hifi", .dai_fmt = SND_SOC_DAIFMT_I2S | SND_SOC_DAIFMT_NB_NF | SND_SOC_DAIFMT_CBS_CFS, .init = pmod_amp3_init, }; static struct snd_soc_card pmod_amp3_card = { .name = "PMOD AMP3 SSM2518", .owner = THIS_MODULE, .dai_link = &pmod_amp3_dai_link, .num_links = 1, .dapm_widgets = pmod_amp3_widgets, .num_dapm_widgets = ARRAY_SIZE(pmod_amp3_widgets), .dapm_routes = pmod_amp3_routes, .num_dapm_routes = ARRAY_SIZE(pmod_amp3_routes), .fully_routed = true, };