This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:sound:adau1373 [16 Nov 2012 13:52] – [Supported Devices] Lars-Peter Clausen | resources:tools-software:linux-drivers:sound:adau1373 [23 Feb 2017 12:47] (current) – Lars-Peter Clausen | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADAU1373 Sound CODEC Linux Driver ====== | ====== ADAU1373 Sound CODEC Linux Driver ====== | ||
+ | |||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
Line 8: | Line 9: | ||
* [[adi> | * [[adi> | ||
- | ====== Source Code ====== | + | ===== Source Code ===== |
==== Status ==== | ==== Status ==== | ||
- | ^ Source | + | ^ Source ^ Mainlined? ^ |
| [[git.linux.org> | | [[git.linux.org> | ||
Line 22: | Line 23: | ||
| include | [[git.linux.org> | | include | [[git.linux.org> | ||
- | ====== Example device initialization | + | ===== Example device initialization ===== |
{{page> | {{page> | ||
Line 182: | Line 183: | ||
^ Name ^ Supported by driver ^ Description ^ | ^ Name ^ Supported by driver ^ Description ^ | ||
- | | SND_SOC_DAIFMT_I2S | + | | SND_SOC_DAIFMT_I2S |
| SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode | | | SND_SOC_DAIFMT_RIGHT_J | yes | Right Justified mode | | ||
| SND_SOC_DAIFMT_LEFT_J | | SND_SOC_DAIFMT_LEFT_J | ||
Line 308: | Line 309: | ||
^ Source | ^ Source | ||
- | | [[bfgit>linux-kernel?sound/ | + | | [[git.linux.org>sound/ |
==== Files ==== | ==== Files ==== | ||
Line 355: | Line 356: | ||
Load the driver and make sure the sound card is properly instantiated. | Load the driver and make sure the sound card is properly instantiated. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> modprobe snd-bf5xx-i2s | root:/> modprobe snd-bf5xx-i2s | ||
Line 364: | Line 365: | ||
asoc: ADAU1373 <-> bf5xx-i2s mapping ok | asoc: ADAU1373 <-> bf5xx-i2s mapping ok | ||
</ | </ | ||
- | </box> | + | </WRAP> |
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> modprobe snd-pcm-oss | root:/> modprobe snd-pcm-oss | ||
Line 376: | Line 377: | ||
Playing WAVE ' | Playing WAVE ' | ||
</ | </ | ||
- | </box> | + | </WRAP> |