This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:sound:ad1835a [11 Mar 2015 11:05] – [Status] fix alignment Lars-Peter Clausen | resources:tools-software:linux-drivers:sound:ad1835a [04 Feb 2021 15:36] (current) – [Driver testing] Michael Hennerich | ||
---|---|---|---|
Line 99: | Line 99: | ||
^ Name ^ Supported by driver ^ Description ^ | ^ Name ^ Supported by driver ^ Description ^ | ||
- | | SND_SOC_DAIFMT_I2S | + | | SND_SOC_DAIFMT_I2S |
| SND_SOC_DAIFMT_RIGHT_J | no | Right Justified mode | | | SND_SOC_DAIFMT_RIGHT_J | no | Right Justified mode | | ||
| SND_SOC_DAIFMT_LEFT_J | | SND_SOC_DAIFMT_LEFT_J | ||
Line 286: | Line 286: | ||
Also you can run " | Also you can run " | ||
- Check to make sure mp3s work (assuming you have built mp3play), | - Check to make sure mp3s work (assuming you have built mp3play), | ||
- | - The first step is to download a mp3 file onto the platform. The '' | + | - The first step is to download a mp3 file onto the platform. The '' |
root:/ | root:/ | ||
</ | </ |