This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:sound:ad1835a [05 Sep 2012 14:23] – [Status] Michael Hennerich | resources:tools-software:linux-drivers:sound:ad1835a [04 Feb 2021 15:36] (current) – [Driver testing] Michael Hennerich | ||
---|---|---|---|
Line 8: | Line 8: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | |||
+ | ===== Evaluation Boards ===== | ||
+ | |||
+ | * [[adi> | ||
====== Source Code ====== | ====== Source Code ====== | ||
Line 13: | Line 17: | ||
==== Status ==== | ==== Status ==== | ||
- | ^ Source ^ Mainline? ^ | + | ^ Source ^ Mainline? ^ |
| [[git.linux.org> | | [[git.linux.org> | ||
Line 95: | Line 99: | ||
^ Name ^ Supported by driver ^ Description ^ | ^ Name ^ Supported by driver ^ Description ^ | ||
- | | SND_SOC_DAIFMT_I2S | + | | SND_SOC_DAIFMT_I2S |
| SND_SOC_DAIFMT_RIGHT_J | no | Right Justified mode | | | SND_SOC_DAIFMT_RIGHT_J | no | Right Justified mode | | ||
| SND_SOC_DAIFMT_LEFT_J | | SND_SOC_DAIFMT_LEFT_J | ||
Line 282: | Line 286: | ||
Also you can run " | Also you can run " | ||
- Check to make sure mp3s work (assuming you have built mp3play), | - Check to make sure mp3s work (assuming you have built mp3play), | ||
- | - The first step is to download a mp3 file onto the platform. The '' | + | - The first step is to download a mp3 file onto the platform. The '' |
root:/ | root:/ | ||
</ | </ |