This is an old revision of the document!
analog@debian:~$ mkdir tools analog@debian:~$ cd tools analog@debian:~/tools$ wget https://armkeil.blob.core.windows.net/developer/Files/downloads/gnu-a/10.3-2021.07/binrel/gcc-arm-10.3-2021.07-x86_64-aarch64-none-linux-gnu.tar.xz analog@debian:~/tools$ tar xvf gcc-arm-10.3-2021.07-x86_64-aarch64-none-linux-gnu.tar.xz analog@debian:~/tools$ export CROSS_COMPILE=/home/analog/tools/gcc-arm-10.3-2021.07-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- analog@debian:~/tools$ cd ~
analog@debian:~$ git clone https://github.com/altera-opensource/arm-trusted-firmware analog@debian:~$ cd ./arm-trusted-firmware analog@debian:~/arm-trusted-firmware$ git checkout rel_socfpga_v2.6.0_22.03.02_pr analog@debian:~/arm-trusted-firmware$ make bl31 PLAT=stratix10 DEPRECATED=1 analog@debian:~/arm-trusted-firmware$ cd ~
analog@debian:~$ git clone https://github.com/altera-opensource/u-boot-socfpga analog@debian:~$ cd ./u-boot-socfpga analog@debian:~/u-boot-socfpga$ git checkout rel_socfpga_v2021.10_22.03.02_pr analog@debian:~/u-boot-socfpga$ ln -sf ../arm-trusted-firmware/build/stratix10/release/bl31.bin . analog@debian:~/u-boot-socfpga$ echo 'CONFIG_BOOTARGS=“earlycon panic=-1 console=ttyS0,115200 root=/dev/mmcblk0p2 rw rootwait”' » configs/socfpga_stratix10_defconfig analog@debian:~/u-boot-socfpga$ echo 'CONFIG_BOOTCOMMAND=“mw.l 0xFFD1102C 0x00000000; setenv ethaddr 00:15:17:ab:cd:ef; load mmc 0:1 ${kernel_addr_r} Image; load mmc 0:1 ${fdt_addr_r} socfpga_stratix10_socdk.dtb; booti ${kernel_addr_r} - ${fdt_addr_r}”' » configs/socfpga_stratix10_defconfig analog@debian:~/u-boot-socfpga$ make socfpga_stratix10_defconfig analog@debian:~/u-boot-socfpga$ sed -i '/4GB/,/0x80000000>;/creg = <0 0x00000000 0 0x80000000>;' arch/arm/dts/socfpga_stratix10_socdk.dts analog@debian:~/u-boot-socfpga$ make analog@debian:~/u-boot-socfpga$ cp u-boot.itb /media/analog/BOOT/ analog@debian:~/u-boot-socfpga$ cd ~
analog@debian:~$ git clone https://github.com/analogdevicesinc/hdl analog@debian:~$ cd hdl/projects/ad9213_dual_ebz/s10soc analog@debian:~/hdl/projects/ad9213_dual_ebz/s10soc$ make Building ad9213_dual_ebz_s10soc [/home/analog/hdl/projects/ad9213_dual_ebz/s10soc/ad9213_dual_ebz_s10soc_quartus.log] ... OK analog@debian:~/hdl/projects/ad9213_dual_ebz/s10soc$ quartus_pfg -c ad9213_dual_ebz_s10soc.sof -o hps_path=../../../../u-boot-socfpga/spl/u-boot-spl-dtb.hex ad9213_dual_ebz_s10soc_hps.sof analog@debian:~/hdl/projects/ad9213_dual_ebz/s10soc$ quartus_pfg -c ad9213_dual_ebz_s10soc_hps.sof ad9213_dual_ebz_s10soc_hps.jic -o device=MT25QU02G -o flash_loader=1SX280LU2F50E2VGS2
SW2 4-bit DIP Switch
Switch Bit | 1 | 2 | 3 | 4 |
Name | MSEL0 | MSEL1 | MSEL2 | Not Used |
JTAG Mode | ON | ON | ON | OFF |
QSPI Mode | ON | OFF | OFF | OFF |