This is an old revision of the document!
Download the pre-build image for you device in question.
Latest Build: 2018_05_08 - 2018_R1
Linux branch:2018_R1
Linux repository:https://github.com/analogdevicesinc/linux.git
Vivado branch:hdl_2018_r1
Vivado repository:https://github.com/analogdevicesinc/hdl.git
FPGA Carrier | FMC Card | Download |
---|
KC705 | AD9467_FMC | 2018_r1_kc705_ad9467_fmc.zip |
KC705 | FMCDAQ2 | 2018_r1_kc705_fmcdaq2.zip |
KC705 | FMCJESDADC1 | 2018_r1_kc705_fmcjesdadc1.zip |
KC705 | FMCOMMS2-3 | 2018_r1_kc705_fmcomms2-3.zip |
KC705 | FMCOMMS4 | 2018_r1_kc705_fmcomms4.zip |
KCU105 | ADRV9371X | 2018_r1_kcu105_adr9371x.zip |
KCU105 | FMCDAQ2 | 2018_r1_kcu105_fmcdaq2.zip |
KCU105 | FMCDAQ3 | 2018_r1_kcu105_fmcdaq3.zip |
KCU105 | FMCOMMS2-3 | 2018_r1_kcu105_fmcomms2-3.zip |
KCU105 | FMCOMMS4 | 2018_r1_kcu105_fmcomms4.zip |
VC707 | AD6676EVB | 2018_r1_vc707_ad6676evb.zip |
VC707 | FMCADC2 | 2018_r1_vc707_fmcadc2.zip |
VC707 | FMCADC5 | 2018_r1_vc707_fmcadc5.zip |
VC707 | FMCDAQ2 | 2018_r1_vc707_fmcdaq2.zip |
VC707 | FMCJESDADC1 | 2018_r1_vc707_fmcjesdadc1.zip |
VC707 | FMCOMMS2-3 | 2018_r1_vc707_fmcomms2-3.zip |
VC707 | FMCOMMS4 | 2018_r1_vc707_fmcomms4.zip |
Build: 2017_08_24 - 2016_R2
Linux SHA:c352b21d2354d0e198c1a5da5b351682ae80e986
Linux branch:2016_R2
Linux repository:https://github.com/analogdevicesinc/linux.git
Vivado SHA:ed12efc6203eb08f9c015eb18e9d0fa4d1fb5a38
Vivado branch:hdl_2016_r2
Vivado repository:https://github.com/analogdevicesinc/hdl.git
FPGA Carrier | FMC Card | Download |
---|---|---|
VC707 | FMCDAQ2 | vc707_fmcdaq2_2016_r2.zip |
Build: 2016_05_26 - 2015_R2
Linux SHA:1610de3ba34b71f774cbe7e8f2131cda037a6230
Linux branch:2015_R2
Linux repository:https://github.com/analogdevicesinc/linux.git
Vivado SHA:1b9182cac07ac80f9d7cc67bc9b30c7670a4f3f3
Vivado branch:hdl_2015_r2
Vivado repository:https://github.com/analogdevicesinc/hdl.git
FPGA Carrier | FMC Card | Download |
---|---|---|
KC705 | AD9467_FMC | kc705_ad9467_fmc_2015_r2.zip |
KC705 | FMCDAQ2 | kc705_fmcdaq2_2015_r2.zip |
KC705 | FMCJESDADC1 | kc705_fmcjesdadc1_2015_r2.zip |
KC705 | FMCOMMS1 | kc705_fmcomms1_2015_r2.zip |
KC705 | FMCOMMS2-3 | kc705_fmcomms2-3_2015_r2.zip |
KCU105 | FMCDAQ2 | kcu105_fmcdaq2_2015_r2.zip |
VC707 | AD6676EVB | vc707_ad6676evb_2015_r2.zip |
VC707 | FMCADC2 | vc707_fmcadc2_2015_r2.zip |
VC707 | FMCADC5 | vc707_fmcadc5_2015_r2.zip |
VC707 | FMCDAQ2 | vc707_fmcdaq2_2015_r2.zip |
VC707 | FMCJESDADC1 | vc707_fmcjesdadc1_2015_r2.zip |
VC707 | FMCOMMS1 | vc707_fmcomms1_2015_r2.zip |
VC707 | FMCOMMS2-3 | vc707_fmcomms2-3_2015_r2.zip |
Build: 2015_06_30 - 2015_R1_PRE
Linux SHA:ef29f1f9900de8f5a7c290cf459498e1f8cc831a
Linux branch:2015_R1
Linux repository:https://github.com/analogdevicesinc/linux.git
HDL SHA:499357a65ac6877c96244bbcf664cbd9440970ce
HDL branch:hdl_2015_r1
HDL repository:https://github.com/analogdevicesinc/hdl.git
FPGA Carrier | FMC Card | Download |
---|---|---|
KC705 | AD9467_FMC | kc705_ad9467_fmc_2015_R1_PRE.zip |
KC705 | FMCDAQ2 | kc705_fmcdaq2_2015_R1_PRE.zip |
KC705 | FMCJESDADC1 | kc705_fmcjesdadc1_2015_R1_PRE.zip |
KC705 | FMCOMMS1 | kc705_fmcomms1_2015_R1_PRE.zip |
KC705 | FMCOMMS2/3 | kc705_fmcomms2-3_2015_R1_PRE.zip |
KCU105 | FMCDAQ2 | kcu105_fmcdaq2_2015_R1_PRE.zip |
VC707 | AD6676 | vc707_ad6676evb_2015_R1_PRE.zip |
VC707 | FMCADC2 | vc707_fmcadc2_2015_R1_PRE.zip |
VC707 | FMCADC5 | vc707_fmcadc5_2015_R1_PRE.zip |
VC707 | FMCDAQ2 | vc707_fmcdaq2_2015_R1_PRE.zip |
VC707 | FMCJESDADC1 | vc707_fmcjesdadc1_2015_R1_PRE.zip |
VC707 | FMCOMMS1 | vc707_fmcomms1_2015_R1_PRE.zip |
VC707 | FMCOMMS2/3 | vc707_fmcomms2-3_2015_R1_PRE.zip |
Build: 2015_05_27 - 2014_R2
Linux SHA:d06f1b2708a4a7d6090703b0f1a3678191bb3aa0
Linux branch:2014_R2
Linux repository:https://github.com/analogdevicesinc/linux.git
HDL SHA:7b8b810c872df170515916b15944b13856646303
HDL branch:hdl_2014_r2
HDL repository:https://github.com/analogdevicesinc/hdl.git
FPGA Carrier | FMC Card | Download |
---|---|---|
KC705 | AD9467_FMC | kc705_ad9467_fmc_2014_R2.zip |
KC705 | FMCDAQ2 | kc705_fmcdaq2_2014_R2.zip |
KC705 | FMCJESDADC1 | kc705_fmcjesdadc1_2014_R2.zip |
KC705 | FMCOMMS1 | kc705_fmcomms1_2014_R2.zip |
KC705 | FMCOMMS2/3 | kc705_fmcomms2-3_2014_R2.zip |
KCU105 | FMCDAQ2 | kcu105_fmcdaq2_2014_R2.zip |
VC707 | FMCADC2 | vc707_fmcadc2_2014_R2.zip |
VC707 | FMCADC5 | vc707_fmcadc5_2014_R2.zip |
VC707 | FMCOMMS2/3 | vc707_fmcomms2-3_2014_R2.zip |
There are two ways of loading the design. One is using the XMD command line. Open a xmd command window/shell and enter the commands manually.
Below is just a example and the file-names may vary.
Xilinx XMD command console
Dave@HAL9000:~$ xmd ****** Xilinx Microprocessor Debugger (XMD) Engine ****** XMD v2014.2 (64-bit) **** SW Build 932637 on Wed Jun 11 13:12:06 MDT 2014 ** Copyright 1986-2014 Xilinx, Inc. All Rights Reserved. XMD% fpga -f download.bit Configuring Device 1 (xcku040) with Bitstream -- download.bit ....10....20....30....40....50....60.....70....80....90....Done Successfully downloaded bit file. JTAG chain configuration -------------------------------------------------- Device ID Code IR Length Part Name 1 03822093 6 xcku040 0 XMD% connect mb mdm JTAG chain configuration -------------------------------------------------- Device ID Code IR Length Part Name 1 03822093 6 xcku040 MicroBlaze Processor Configuration : ------------------------------------- Version............................9.3 Optimization.......................Performance Interconnect.......................AXI-LE MMU Type...........................Full_MMU No of PC Breakpoints...............1 No of Read Addr/Data Watchpoints...0 No of Write Addr/Data Watchpoints..0 Instruction Cache Support..........on Instruction Cache Base Address.....0x80000000 Instruction Cache High Address.....0xbfffffff Data Cache Support.................on Data Cache Base Address............0x80000000 Data Cache High Address............0xbfffffff Exceptions Support................on FPU Support.......................off Hard Divider Support...............on Hard Multiplier Support............on - (Mul64) Barrel Shifter Support.............on MSR clr/set Instruction Support....on Compare Instruction Support........on PVR Supported......................on PVR Configuration Type.............Full Data Cache Write-back Support......off Fault Tolerance Support............off Stack Protection Support...........off Connected to "mb" target. id = 0 Starting GDB server for "mb" target (id = 0) at TCP port no 1234 XMD% dow /home/dace/linux/arch/microblaze/boot/simpleImage.kcu105_ad_fmcdaq2_ebz System Reset .... DONE Downloading Program -- /home/michael/linux/arch/microblaze/boot/simpleImage.kcu105_ad_fmcdaq2_ebz section, .text: 0x80000000-0x8031cda7 section, .init.text: 0x803fc000-0x804185eb section, .init.ivt: 0x8041afac-0x8041afd3 section, __fdt_blob: 0x8031cda8-0x80324da7 section, .rodata: 0x80325000-0x803b950f section, __ksymtab: 0x803b9510-0x803be90f section, __ksymtab_gpl: 0x803be910-0x803c1e27 section, __ksymtab_strings: 0x803c1e28-0x803d4dd7 section, __param: 0x803d4dd8-0x803d5147 section, __modver: 0x803d5148-0x803d5fff section, __ex_table: 0x803d6000-0x803d75df section, .notes: 0x803d75e0-0x803d7603 section, .sdata2: 0x803d7604-0x803d7fff section, .data: 0x803d8000-0x803fbc5f section, .init.data: 0x804185ec-0x8041afab section, .init.setup: 0x8041afd4-0x8041b327 section, .initcall.init: 0x8041b328-0x8041b683 section, .con_initcall.init: 0x8041b684-0x8041b68b section, .init.ramfs: 0x8041b68c-0x806f97b3 section, .bss: 0x806fa000-0x8070f8db Download Progress........10.......20.......30.......40.......50........60.......70.......80.......90........Done Setting PC with Program Start Address 0x80000000 XMD% con Processor started. Type "stop" to stop processor RUNNING> XMD%
XMD has been replaced with XSCT/XSDB in newer releases of VIVADO. In windows, you can run the XSCT terminal from start menu → Xilinx Design Tools → Xilinx Software Command Line Tool…
Xilinx XSCT command console
****** Xilinx Software Commandline Tool (XSCT) v2018.2 **** Build date : Jun 14 2018-20:42:51 ** Copyright 1986-2018 Xilinx, Inc. All Rights Reserved. xsct% connect attempting to launch hw_server ****** Xilinx hw_server v2018.2 **** Build date : Jun 14 2018-20:42:52 ** Copyright 1986-2018 Xilinx, Inc. All Rights Reserved. INFO: hw_server application started INFO: Use Ctrl-C to exit hw_server application INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121 tcfchan#0 xsct% fpga -f "c:/Users/kjimenez/Documents/system_top.bit" 100% 8MB 1.7MB/s 00:04 xsct% targets 1 xc7vx485t 2 MicroBlaze Debug Module at USER2 3 MicroBlaze #0 (Running) xsct% target 3 xsct% dow "c:/Users/kjimenez/Documents/simpleImage.vc707_fmcomms2-3" Downloading Program -- C:/Users/kjimenez/Documents/simpleImage.vc707_fmcomms2-3 section, .text: 0x80000000 - 0x8040f40b section, __fdt_blob: 0x8040f40c - 0x8041f40b section, .rodata: 0x80420000 - 0x80570057 section, .builtin_fw: 0x80570058 - 0x8057007b section, __ksymtab: 0x8057007c - 0x80576063 section, __ksymtab_gpl: 0x80576064 - 0x8057abd3 section, __ksymtab_strings: 0x8057abd4 - 0x80593b87 section, __param: 0x80593b88 - 0x8059405f section, __modver: 0x80594060 - 0x80594fff section, __ex_table: 0x80595000 - 0x805965a7 section, .notes: 0x805965a8 - 0x805965cb section, .sdata2: 0x805965cc - 0x80596fff section, .data: 0x80597000 - 0x805ba19f section, .init.text: 0x805bb000 - 0x805dbf7b section, .init.data: 0x805dbf80 - 0x805ddc5f section, .init.ivt: 0x805ddc60 - 0x805ddc87 section, .init.setup: 0x805ddc88 - 0x805ddfdb section, .initcall.init: 0x805ddfdc - 0x805de3bf section, .con_initcall.init: 0x805de3c0 - 0x805de3c3 section, .init.ramfs: 0x805de3c4 - 0x808f226b section, .bss: 0x808f3000 - 0x8090b823 100% 8MB 0.2MB/s 00:46 Setting PC to Program Start Address 0x80000000 Successfully downloaded C:/Users/kjimenez/Documents/simpleImage.vc707_fmcomms2-3 xsct% Info: MicroBlaze #0 (target 3) Stopped at 0x0 (Stop) xsct% con Info: MicroBlaze #0 (target 3) Running xsct%
The second method is to run the tcl script which takes care of loading the bit file and the linux image. Run Vivado TCL Shell from Windows start menu → Xilinx Design Suite → Vivado → Vivado TCL Shell. (In Linux, source the settings.sh file first)
Then run the tcl script:
Vivado TCL shell or Linux console
****** Vivado v2014.2 (64-bit) **** SW Build 932637 on Wed Jun 11 13:33:10 MDT 2014 **** IP Build 924643 on Fri May 30 09:20:16 MDT 2014 ** Copyright 1986-2014 Xilinx, Inc. All Rights Reserved. Vivado% xmd -tcl run.tcl ****** Xilinx Microprocessor Debugger (XMD) EngineExecuting user script : run.tcl ****** XMD v2014.2 (64-bit) **** SW Build 932637 on Wed Jun 11 13:12:06 MDT 2014 ** Copyright 1986-2014 Xilinx, Inc. All Rights Reserved. Configuring Device 1 (xcku040) with Bitstream -- daq2_kcu105.sdk/SDK/SDK_Export/hw/system_top.bit ..............................................................10..............................................................20.............................................................30..............................................................40.............................................................50..............................................................60.............................................................70..............................................................80.............................................................90..............................................................Done Successfully downloaded bit file. JTAG chain configuration -------------------------------------------------- Device ID Code IR Length Part Name 1 03822093 6 xcku040 JTAG chain configuration -------------------------------------------------- Device ID Code IR Length Part Name 1 03822093 6 xcku040 MicroBlaze Processor Configuration : ------------------------------------- Version............................9.3 Optimization.......................Performance Interconnect.......................AXI-LE MMU Type...........................Full_MMU No of PC Breakpoints...............1 No of Read Addr/Data Watchpoints...0 No of Write Addr/Data Watchpoints..0 Instruction Cache Support..........on Instruction Cache Base Address.....0x80000000 Instruction Cache High Address.....0xbfffffff Data Cache Support.................on Data Cache Base Address............0x80000000 Data Cache High Address............0xbfffffff Exceptions Support................on FPU Support.......................off Hard Divider Support...............on Hard Multiplier Support............on - (Mul64) Barrel Shifter Support.............on MSR clr/set Instruction Support....on Compare Instruction Support........on PVR Supported......................on PVR Configuration Type.............Full Data Cache Write-back Support......off Fault Tolerance Support............off Stack Protection Support...........off Connected to "mb" target. id = 0 Starting GDB server for "mb" target (id = 0) at TCP port no 1234 Processor stopped System Reset .... DONE Downloading Program -- simpleImage.kcu105_fmcdaq2 section, .text: 0x80000000-0x80323fe7 section, .init.text: 0x80409000-0x8042598f section, .init.ivt: 0x8042834c-0x80428373 section, __fdt_blob: 0x80323fe8-0x8032bfe7 section, .rodata: 0x8032c000-0x803c40d7 section, .builtin_fw: 0x803c40d8-0x803c40ef section, __ksymtab: 0x803c40f0-0x803c94ef section, __ksymtab_gpl: 0x803c94f0-0x803ccc77 section, __ksymtab_strings: 0x803ccc78-0x803e0427 section, __param: 0x803e0428-0x803e0797 section, __modver: 0x803e0798-0x803e0fff section, __ex_table: 0x803e1000-0x803e25df section, .notes: 0x803e25e0-0x803e2603 section, .sdata2: 0x803e2604-0x803e2fff section, .data: 0x803e3000-0x8040807f section, .init.data: 0x80425990-0x8042834b section, .init.setup: 0x80428374-0x804286c7 section, .initcall.init: 0x804286c8-0x80428a33 section, .con_initcall.init: 0x80428a34-0x80428a3b section, .init.ramfs: 0x80428a3c-0x809e2243 section, .bss: 0x809e3000-0x809f89bb Download Progress...........10..........20..........30..........40..........50..........60...........70..........80..........90..........Done Setting PC with Program Start Address 0x80000000 RUNNING> Disconnected from Target 0 Processor started. Type "stop" to stop processor
If you are interested in the Linux console messages and command line interface, connect a USB cable to the USB UART port. Terminal settings are 115200,8N1.
There are two users:
user | password |
---|---|
root | analog |
analog | analog |
If you FPGA carrier board (KC705, vc707, ml605) features a LCD display and the board is connected to a DHCP enabled network. You should also see it's IP address printed on the display. This allows you to connect remote to the board as well. (ssh, libiio remote)
Unlike shown in the picture below you won't see the second line. In case the IP address is 192.168.2.2, this indicates that DHCP failed and it's now using it's default address. This address may not be within your subnet, and things therefore may fail.
You should see the kernel start-up messages as follows: