This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:networking-mac802154:adf7242 [24 Nov 2017 13:23] – [Firmware for Automatic IEEE 802.15.4 Operating Modes (AN-1082)] Michael Hennerich | resources:tools-software:linux-drivers:networking-mac802154:adf7242 [19 Jan 2018 10:28] – rename xcomm_zynq -> master Alexandru Ardelean | ||
---|---|---|---|
Line 4: | Line 4: | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
Line 22: | Line 23: | ||
^ Function ^ File ^ | ^ Function ^ File ^ | ||
- | | driver | + | | driver |
- | | include | [[linux.github> | + | | include | [[linux.github> |
===== Firmware for Automatic IEEE 802.15.4 Operating Modes (AN-1082) ===== | ===== Firmware for Automatic IEEE 802.15.4 Operating Modes (AN-1082) ===== | ||
Line 102: | Line 103: | ||
Alternatively, | Alternatively, | ||
- | \\ Read the [[linux.github> | + | \\ Read the [[linux.github> |
Example: | Example: |