This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:net-phy:adin [22 Oct 2020 11:03] – update title Alexandru Ardelean | resources:tools-software:linux-drivers:net-phy:adin [03 Jan 2021 21:46] – fix links Robin Getz | ||
---|---|---|---|
Line 40: | Line 40: | ||
Depending on the MAC driver that is used and the operating mode (MII, RGMII, RMII), a device-tree entry for the PHY may or may-not be needed. | Depending on the MAC driver that is used and the operating mode (MII, RGMII, RMII), a device-tree entry for the PHY may or may-not be needed. | ||
- | The PHY can be configured via HW pins ([[https:// | + | The PHY can be configured via HW pins ([[adi>media/ |
**Optional properties (for MAC):** | **Optional properties (for MAC):** |