The ADIN1100 is a low power single port 10BASE-T1L transceiver designed for industrial Ethernet applications and is compliant with the IEEE 802.3cg Ethernet standard for long reach 10 Mb/s Single Pair Ethernet. It integrates an Ethernet PHY core with all the associated analog circuitry, input and output clock buffering, the management interface control register and subsystem registers, as well as the MAC interface and control logic to manage the reset and clock control and pin configuration.
The PHY core supports the 1.0 V pk-pk operating mode and the 2.4 V pk-pk operating mode defined in the standard and can operate from a single power supply rail of 1.8V or 3.3V, with the lower voltage option supporting the 1.0 V pk-pk transmit voltage level.
The 1.0 V pk-pk operating mode, external termination resistors and independent Rx/Tx pins make the ADIN1100 suited to intrinsic safety applications.
The ADIN1100 has an integrated voltage supply monitoring circuit and power on reset circuitry to improve system level robustness.
The MDIO interface is a two-wire serial interface for communication between a host processor or MAC and the ADIN1100, thereby allowing access to control and status information in the PHY core management registers. This interface is compatible with both the IEEE 802.3 Standard Clause 22 and Clause 45 management frame structures.
The ADIN1100 is available in a 6 mm × 6 mm 40-ld package.
Source | Mainlined? |
---|---|
drivers/net/phy/adin1100.c | In Progress |
Function | File |
---|---|
driver | drivers/net/phy/adin1100.c |
The ADIN 10BASE-T1L PHY driver instantiates via Linux's phylib framework, which is typically enabled on most systems.
Depending on the MAC driver that is used and the operating mode (MII, RMII), a device-tree entry for the PHY may or may-not be needed. The PHY can be configured via HW pins (see datasheet).
Optional properties (for MAC):
Example: ethernet-mac0 { #address-cells = <1>; #size-cells = <0>; phy-mode = "mii"; ethernet-phy@0 { reg = <0>; }; }; ethernet-mac1 { #address-cells = <1>; #size-cells = <0>; phy-mode = "rmii"; ethernet-phy@1 { reg = <1>; }; };
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Symbol: ADIN1100_PHY [=y] Type : tristate Prompt: Analog Devices Industrial Ethernet 10BASE-T1L PHYs Location: -> Device Drivers -> Network device support (NETDEVICES [=y])│ (1) -> PHY Device support and infrastructure (PHYLIB [=y]) Defined at drivers/net/phy/Kconfig:208 Depends on: NETDEVICES [=y] && PHYLIB [=y]
This requires that another 10BASE-T1L PHY be connected to the other end of the network cable, or that a media converter be used to convert to normal twisted-pair ethernet that standard ethernet cables use.
If NetworkManager isn't running, it sometimes works to obtain a DHCP lease via dhclient eth0 [or eth1 or eth2, depending which MAC is attached to the ADIN 10BASE-T1L PHY].
This tool will display the general status of the available network interfaces. If they’ve obtained an IP address, RX packets/errors/dropped/etc, TX packets/errors/dropped/etc, MAC address, etc.
Typically, if both TX & RX values are incremented, it means that it is working. Also note that there are error counters; if only the TX/RX counters increment, something may be wrong in the configuration between MAC & PHY, or sometimes at the physical configuration (i.e. clocks not working, pins not connected properly, etc).
root@analog:~# ifconfig eth0 Link encap:Ethernet HWaddr d6:41:50:ed:3b:65 UP BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:609895 errors:5 dropped:0 overruns:0 frame:0 TX packets:286926 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (647.6 MB) TX bytes:0 (38.7 MB) Interrupt:23 eth1 Link encap:Ethernet HWaddr 00:0a:35:03:73:d9 UP BROADCAST MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:0 (0.0 B) Interrupt:24 lo Link encap:Local Loopback inet addr:127.0.0.1 Mask:255.0.0.0 inet6 addr: ::1/128 Scope:Host UP LOOPBACK RUNNING MTU:65536 Metric:1 RX packets:8 errors:0 dropped:0 overruns:0 frame:0 TX packets:8 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:480 (480.0 B) TX bytes:480 (480.0 B)
This tool queries the MAC & PHY via the MAC driver. The MAC driver should also allows access to the PHY registers.
ethtool can be used to show & override link settings and other parameters for the MAC & PHY.
Links for the tool:
root@analog:~# ethtool eth0 Settings for eth0: Supported ports: [ TP MII ] Supported link modes: 10baseT/Full Supported pause frame use: No Supports auto-negotiation: Yes Supported FEC modes: Not reported Advertised link modes: 10baseT/Full Advertised pause frame use: No Advertised auto-negotiation: Yes Advertised FEC modes: Not reported Link partner advertised link modes: 10baseT/Full Link partner advertised pause frame use: Symmetric Link partner advertised auto-negotiation: Yes Link partner advertised FEC modes: Not reported Speed: 10Mb/s Duplex: Full Port: MII PHYAD: 0 Transceiver: internal Auto-negotiation: on Link detected: yes
Since the PHY can only do 10 Mbps full-duplex, the only operation possible here is to disable auto-negotiation and set preferred/forced master/slave
ethtool -s eth0 speed 10 duplex full master-slave forced-master ethtool -s eth0 speed 10 duplex full master-slave forced-slave ethtool -s eth0 autoneg on ethtool -s eth0 autoneg on master-slave preferred-master ethtool -s eth0 autoneg on master-slave preferred-slave ethtool -s eth0 autoneg on master-slave forced-master ethtool -s eth0 autoneg on master-slave forced-slave
ADIN1100 supports multiple cable diagnostics options. Some of them could not be added in the driver as ethtool ops.
If you want control over those features from C code, add those files to your project:
Function | File |
---|---|
Header | adin10spe_phy.h |
Code | adin10spe_phy.c |
Or you can compile the tool:
root@analog:~/adin1100# cmake CMakeLists.txt -- The C compiler identification is GNU 8.3.0 -- Check for working C compiler: /usr/bin/cc -- Check for working C compiler: /usr/bin/cc -- works -- Detecting C compiler ABI info -- Detecting C compiler ABI info - done -- Detecting C compile features -- Detecting C compile features - done -- Configuring done -- Generating done -- Build files have been written to: /root/adin1100 root@analog:~/adin1100# make Scanning dependencies of target adin10spe_phy_tool [ 33%] Building C object CMakeFiles/adin10spe_phy_tool.dir/adin10spe_phy.c.o [ 66%] Building C object CMakeFiles/adin10spe_phy_tool.dir/adin10spe_phy_tool.c.o [100%] Linking C executable adin10spe_phy_tool [100%] Built target adin10spe_phy_tool root@analog:~/adin1100# ls CMakeCache.txt CMakeFiles CMakeLists.txt Makefile adin10spe_phy.c adin10spe_phy.h adin10spe_phy_tool adin10spe_phy_tool.c cmake_install.cmake root@analog:~/adin1100#
Check command line formatting via:
root@analog:~/adin1100# ./adin10spe_phy_tool help ADIN10SPE_PHY cable diagnostics control tool: Usage: adin10spe_phy_tool [interface name] [phy ID] [start-fg | stop-fg | start-test | stop-test | start-lb | stop-lb] ... Example: adin10spe_phy_tool eth1 0 start-loopback pcs-loopback Features: Frame Generator: Usage: adin10spe_phy_tool [interface name] [phy ID] [start-fg | stop-fg] [frame-control] [frame-output-mode] [frame-length] [inter-frame-gap] [frames-number] frame-control: random-payload zeros-payload ones-payload alternating-ones-payload decrementing-bytes-payload frame-output-mode: continous-mode burst-mode Example 1: adin10spe_phy_tool eth1 0 start-fg ones-payload burst-mode 100 50 10 Example 2: adin10spe_phy_tool eth1 0 stop-fg Test mode: Usage: adin10spe_phy_tool [interface name] [phy ID] [start-test | stop-test] [test-mode] test-mode: test1: repeatedly transmits the data symbol sequence (+1, –1) test2: transmits ten “+1” symbols followed by ten “-1” symbols test3: transmits as in non-test operation and in the master data mode Example 1: adin10spe_phy_tool eth1 0 start-test test2 Example 2: adin10spe_phy_tool eth1 0 stop-test Loopback: Usage: adin10spe_phy_tool [interface name] [phy ID] [start-lb | stop-lb] [lb-mode] lb-mode: pma-loopback pcs-loopback mac-loopback Example 1: adin10spe_phy_tool eth1 0 start-lb pcs-loopback Example 2: adin10spe_phy_tool eth1 0 stop-lb Software power-down: Usage: adin10spe_phy_tool [interface name] [phy ID] software-power-down [True | False] Example : adin10spe_phy_tool eth1 0 software-power-down True root@analog:~/adin1100#
This is a more system-general test but it also validates the PHY.
On one of the endpoints with the ADIN1100, run:
iperf -s
and on another system
iperf -c <ip-addr-of-the-other-system>
Then reverse the commands on the hosts. iperf only works in one direction.
One one side, generate a file with random data (say 1GB)
dd if=/dev/urandom of=test.data bs=1M count=1000 sha256sum test.data <SHA256-hash-of-data>
Then transfer the data to the other side with scp,ftp,etc:
scp test.data root@<ip-addr-of-the-other-host>
On the other host check the hash
sha256sum test.data <SHA256-hash-of-data> == should be identical with the first hash