The ADIN1110 is a low power single port 10BASE-T1L MACPHY designed for industrial Ethernet applications. It integrates an Ethernet PHY core with a MAC and all the associated analog circuitry, input and output clock buffering.
Programmable transmit levels, external termination resistors and independent Rx/Tx pins make the ADIN1110 suited to intrinsic safety applications. The ADIN1110 has an integrated voltage supply monitoring and power on reset circuitry to improve system level robustness.
The device has a 4-wire SPI interface for communication between the MAC and host processor.
Source | Mainlined? |
adin1110.c | Yes |
Function | File |
---|---|
driver | drivers/net/ethernet/adi/adin1110.c |
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Symbol: ADIN1110 [=y] Type : tristate Prompt: Analog Devices ADIN1110 MAC-PHY Location: -> Device Drivers -> Network device support (NETDEVICES [=y]) -> Ethernet driver support (ETHERNET [=y]) (1) -> Analog Devices devices (NET_VENDOR_ADI [=y]) Defined at drivers/net/ethernet/adi/Kconfig:20 Depends on: NETDEVICES [=y] && ETHERNET [=y] && NET_VENDOR_ADI [=y] && SPI [=y] Selects: CRC8 [=y]
This requires that another 10BASE-T1L PHY be connected to the other end of the network cable, or that a media converter be used to convert to normal twisted-pair ethernet that standard ethernet cables use.
ADIN1110 communicates with the host via SPI. For 10 Mbps bandwidth, SPI frequency needs to be around 23 MHz. Lower SPI frequencies are supported but will result in a lower bandwidth. At 1 MHz the MAC will provide aprox. 0.4 Mbps of bandwidth.
Connect to host the SCLK, CS_N, SDI, SDO and INT_N. (The INT_N is mandatory, see DT bindings). RX frames and sent TX frames are signaled to the host by INT_N IRQ pin.
ADIN1110 probes via devicetree.
ethernet@0 { compatible = "adi,adin1110"; /* SPI CS number */ reg = <0>; /* will need 23 MHz for 10 Mbps, lower speeds will result in lower bandwidth */ spi-max-frequency = <1000000>; /* optional, will check all control read/writes over SPI */ adi,spi-crc; #address-cells = <1>; #size-cells = <0>; /* an IRQ is required, INT_N pin is configured to signal RX/TX frames */ interrupt-parent = <&gpio>; interrupts = <25 2>; /* This is the host MAC address, by default ADIN1110 will also accept broadcast frames */ mac-address = [ CA 2F B7 10 23 63 ]; phy@0 { compatible = "ethernet-phy-id0283.bc91"; reg = <0x0>; }; };
This tool will display the general status of the available network interfaces. If they’ve obtained an IP address, RX packets/errors/dropped/etc, TX packets/errors/dropped/etc, MAC address, etc.
Typically, if both TX & RX values are incremented, it means that it is working. Also note that there are error counters; if only the TX/RX counters increment, something may be wrong with the network connection. Check error/dropped counters too.
root@analog:~# ifconfig eth1 eth1: flags=4163<UP,BROADCAST,RUNNING,MULTICAST> mtu 1500 inet 192.168.160.160 netmask 255.255.255.0 broadcast 192.168.160.255 inet6 fe80::c82f:b7ff:fe10:2363 prefixlen 64 scopeid 0x20<link> ether ca:2f:b7:10:23:63 txqueuelen 1000 (Ethernet) RX packets 132 bytes 8548 (8.3 KiB) RX errors 0 dropped 0 overruns 0 frame 0 TX packets 79 bytes 9943 (9.7 KiB) TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0 device interrupt 55
This tool queries the MAC & PHY via the MAC driver. The MAC driver also allows access to the PHY registers. ethtool can be used to show & override link settings and other parameters for the MAC & PHY.
Links for the tool:
Settings for eth1: Supported ports: [ TP MII ] Supported link modes: 10baseT/Full Supported pause frame use: Symmetric Receive-only Supports auto-negotiation: Yes Supported FEC modes: Not reported Advertised link modes: 10baseT/Full Advertised pause frame use: No Advertised auto-negotiation: Yes Advertised FEC modes: Not reported Link partner advertised link modes: 10baseT/Full Link partner advertised pause frame use: No Link partner advertised auto-negotiation: Yes Link partner advertised FEC modes: Not reported Speed: 10Mb/s Duplex: Full Port: MII PHYAD: 0 Transceiver: internal Auto-negotiation: on Link detected: yes
Since the PHY can only do 10 Mbps full-duplex, the only operation possible here is to disable auto-negotiation and set preferred/forced master/slave
ethtool -s eth1 speed 10 duplex full master-slave forced-master ethtool -s eth1 speed 10 duplex full master-slave forced-slave ethtool -s eth1 autoneg on ethtool -s eth1 autoneg on master-slave preferred-master ethtool -s eth1 autoneg on master-slave preferred-slave ethtool -s eth1 autoneg on master-slave forced-master ethtool -s eth1 autoneg on master-slave forced-slave
root@analog:~# ethtool --phy-statistics eth1 PHY statistics: total_frames_error_count: 0 total_frames_count: 133 length_error_frames_count: 0 alignment_error_frames_count: 0 symbol_error_count: 0 oversized_frames_count: 0 undersized_frames_count: 0 odd_nibble_frames_count: 0 odd_preamble_packet_count: 0 false_carrier_events_count: 0
This is a more system-general test but it also validates the PHY.
On one of the endpoints with the ADIN1300, run:
iperf -s
and on another system
iperf -c <ip-addr-of-the-other-system>
Then reverse the commands on the hosts. iperf only works in one direction.
One one side, generate a file with random data (say 1GB)
dd if=/dev/urandom of=test.data bs=1M count=1000 sha256sum test.data <SHA256-hash-of-data>
Then transfer the data to the other side with scp,ftp,etc:
scp test.data root@<ip-addr-of-the-other-host>
On the other host check the hash
sha256sum test.data <SHA256-hash-of-data> == should be identical with the first hash