This is an old revision of the document!
The ADP5520/01 driver utilizes several Linux device-driver subsystems and provides various software interfaces. It is therefore implemented as a multifunction device (MFD). In this particular case the ADP5520 backlight driver and I/O expander, concurrently leverages the Linux backlight, LED, GPIO, and input subsystems for its keypad functionality.
The ADP5520/01 core driver in drivers/mfd provides common services for the subsystem drivers. These services include register access, control and shared interrupt management.
The core registers/enumerates platform devices for the various subsystems via the platform device and driver system.
When a platform driver for one of the subsystems is instantiated, the core initializes the chip (which may be specified by the platform data).
The ADP5520/01 platform drivers follow the standard driver model convention, where discovery/enumeration is handled outside the drivers, and drivers provide probe() and remove() methods.
Each peripheral (subsystem device) has a view of the device which is implicitly narrowed to the specific set of resources that peripheral requires in order to function correctly.
The device driver uses a set of platform data to pass configurations through to the core and the subsidiary drivers so that there can be support for multiple ADP5520/01 devices built into a single kernel image.
Backlight:
LED:
Keypad:
GPIO:
Function | File |
---|---|
MFD-CORE | drivers/mfd/adp5520.c |
include | include/linux/mfd/adp5520.h |
BACKLIGHT | drivers/video/backlight/adp5520_bl.c |
LED | drivers/led/leds-adp5520.c |
GPIO | drivers/gpio/adp5520-gpio.c1) |
KEYPAD | drivers/input/keyboard/adp5520-keys.c2) |
ADP5520 PIN | R3 | R2 | R1 | R0 | C0 | C1 | C2 | C3 |
---|---|---|---|---|---|---|---|---|
GPIO | GPIO_R3 | GPIO_R2 | GPIO_R1 | GPIO_R0 | GPIO_C0 | GPIO_C1 | GPIO_C2 | GPIO_C3 |
Keypad | ROW_R3 | ROW_R2 | ROW_R1 | ROW_R0 | COL_C0 | COL_C1 | COL_C2 | COL_C3 |
LED | LED3 | LED2 |
<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_backlight_data{} c linux-kernel>
<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_leds[] c linux-kernel>
<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_leds_data{} c linux-kernel>
<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_gpio_data{} c linux-kernel>
<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_keymap[] c linux-kernel> <source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_keys_data{} c linux-kernel>
<source trunk/arch/blackfin/mach-bf537/boards/stamp.c:adp5520_pdev_data{} c linux-kernel> <source trunk/arch/blackfin/mach-bf537/boards/stamp.c:/CONFIG_PMIC_ADP5520/2-/#if/ c linux-kernel>
Fist of all you need to enable i2c support followed by the ADP5520 MFD Core Driver. Then you may select individual components like LCD backlight, LEDs, GPIOs and Keypad under the corresponding menus.
Device Drivers ---> <*> I2C support ---> <*> Blackfin TWI I2C support Or: <*> GPIO-based bitbanging I2C Device Drivers ---> Multifunction device drivers ---> [*] Analog Devices ADP5520/01 MFD PMIC Core Support
Device Drivers ---> Graphics support ---> [*] Backlight & LCD device support ---> <*> Lowlevel Backlight controls <M> Backlight Driver for ADP5520/ADP5501 using WLED
Device Drivers ---> [*] LED Support ---> <*> LED Class Support <M> LED Support for ADP5520/ADP5501 PMIC
Device Drivers ---> [*] GPIO Support ---> [*] /sys/class/gpio/... (sysfs interface) <M> GPIO Support for ADP5520 PMIC
Device Drivers ---> Input device support ---> <*> Generic input layer (needed for keyboard, mouse, ...) <*> Event interface [*] Keyboards ---> <M> Keypad Support for ADP5520 PMIC
There is no dedicated Blackfin STAMP evaluation board for the ADP5520. During test and driver development we used the ADP5520 Demo Mother/Daughter Board. Connect the ADP5520 Demo Mother to an USB port.
It can be easily wired to the Blackfin STAMP TWI/I2C header.
BF537-STAMP (P10) TWI/I2C header | ADP5520 Daughter Board | |
---|---|---|
PIN | Function | PIN/Function |
5 | SCL | SCL |
6 | SDA | SDA |
10 | GPIO_PG0 | nINT |
20 | GND | GND |
root:/> modprobe adp5520_bl root:/> root:/> cd sys/class/backlight/adp5520-backlight/ root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/backlight/adp5520-backlight> ls -l -r--r--r-- 1 root root 4096 Nov 12 10:31 actual_brightness -rw-r--r-- 1 root root 4096 Nov 12 10:31 bl_power -rw-r--r-- 1 root root 4096 Nov 12 10:31 brightness -rw-rw-r-- 1 root root 4096 Nov 12 10:31 dark_dim -rw-rw-r-- 1 root root 4096 Nov 12 10:31 dark_max -rw-rw-r-- 1 root root 4096 Nov 12 10:31 daylight_dim -rw-rw-r-- 1 root root 4096 Nov 12 10:31 daylight_max lrwxrwxrwx 1 root root 0 Nov 12 10:31 device -> ../../../0-0032 -r--r--r-- 1 root root 4096 Nov 12 10:31 max_brightness -rw-rw-r-- 1 root root 4096 Nov 12 10:31 office_dim -rw-rw-r-- 1 root root 4096 Nov 12 10:31 office_max drwxr-xr-x 2 root root 0 Nov 12 10:31 power lrwxrwxrwx 1 root root 0 Nov 12 10:31 subsystem -> ../../../../../../../../class/backlight root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/backlight/adp5520-backlight> echo 127 > brightness root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/backlight/adp5520-backlight> echo 50 > brightness root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/backlight/adp5520-backlight> echo 0 > brightness
For more information on Backlight handling in Linux read: Documentation/ABI/stable/sysfs-class-backlight
root:/> modprobe leds-adp5520 Registered led device: adp5520-led1 Registered led device: adp5520-led2 Registered led device: adp5520-led3 root:/> cd sys/class/leds/adp5520-led sys/class/leds/adp5520-led1/ sys/class/leds/adp5520-led3/ sys/class/leds/adp5520-led2/ root:/> cd sys/class/leds/adp5520-led1 root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/leds/adp5520-led1> ls -l -rw-r--r-- 1 root root 4096 Nov 12 10:34 brightness lrwxrwxrwx 1 root root 0 Nov 12 10:34 device -> ../../../0-0032 drwxr-xr-x 2 root root 0 Nov 12 10:34 power lrwxrwxrwx 1 root root 0 Nov 12 10:34 subsystem -> ../../../../../../../../class/leds -rw-r--r-- 1 root root 4096 Nov 12 10:34 trigger root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/leds/adp5520-led1> echo 10 > brightness root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/leds/adp5520-led1> echo 255 > brightness root:/sys/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/leds/adp5520-led1> echo 0 > brightness root:/> modprobe -r leds-adp5520 root:/>
For more information on LEDs handling in Linux read: Documentation/leds-class.txt
root:/> modprobe adp5520-gpio root:/> cd sys/class/gpio/gpiochip50/ root:/sys/devices/virtual/gpio/gpiochip50> ls -l -r--r--r-- 1 root root 4096 Nov 12 10:37 base -r--r--r-- 1 root root 4096 Nov 12 10:37 label -r--r--r-- 1 root root 4096 Nov 12 10:37 ngpio drwxr-xr-x 2 root root 0 Nov 12 10:37 power lrwxrwxrwx 1 root root 0 Nov 12 10:37 subsystem -> ../../../../class/gpio -rw-r--r-- 1 root root 4096 Nov 12 10:37 uevent root:/sys/devices/virtual/gpio/gpiochip50> cd root:/>Note that you will have to enable the event_test utility under “Blackfin test programs” in your user space configuration.
--- Blackfin test programs [*] Input event device test
For more information on GPIO handling in Linux read: Documentation/gpio.txt
root:/> modprobe adp5520-keys input: adp5520-keys as /devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/adp5520-keys.5520/input/input0 root:/> event_test /dev/input/event0 Input driver version is 1.0.0 Input device ID: bus 0x18 vendor 0x1 product 0x5520 version 0x1 Input device name: "adp5520-keys" Supported events: Event type 0 (Reset) Event code 0 (Reset) Event code 1 (Key) Event type 1 (Key) Event code 2 (1) Event code 3 (2) Event code 4 (3) Event code 5 (4) Event code 6 (5) Event code 7 (6) Event code 8 (7) Event code 9 (8) Event code 10 (9) Event code 11 (0) Event code 12 (Minus) Event code 13 (Equal) Event code 28 (Enter) Event code 41 (Grave) Event code 43 (BackSlash) Testing ... (interrupt to exit) Event: time 1415788674.340000, type 1 (Key), code 41 (Grave), value 1 Event: time 1415788674.340000, type 0 (Reset), code 0 (Reset), value 0 Event: time 1415788674.516000, type 1 (Key), code 41 (Grave), value 0 Event: time 1415788674.516000, type 0 (Reset), code 0 (Reset), value 0 Event: time 1415788674.912000, type 1 (Key), code 2 (1), value 1 Event: time 1415788674.912000, type 0 (Reset), code 0 (Reset), value 0 Event: time 1415788675.140000, type 1 (Key), code 2 (1), value 0 Event: time 1415788675.140000, type 0 (Reset), code 0 (Reset), value 0 Event: time 1415788675.892000, type 1 (Key), code 6 (5), value 1 Event: time 1415788675.892000, type 0 (Reset), code 0 (Reset), value 0 Event: time 1415788676.092000, type 1 (Key), code 6 (5), value 0 Event: time 1415788676.092000, type 0 (Reset), code 0 (Reset), value 0 root:/> modprobe -r adp5520-keys root:/>
For more information on Input handling in Linux read: Documentation/input/input.txt