This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:multifunction-device:adp5520 [06 May 2011 23:24] – software:driver:linux:adp5520 renamed to resources:tools-software:linux-drivers:multifunction-device:adp5520 andyr | resources:tools-software:linux-drivers:multifunction-device:adp5520 [08 Nov 2011 17:26] – [Supported Devices] Michael Hennerich | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== ADP5520/ | + | ====== ADP5520/ |
===== Supported Devices ===== | ===== Supported Devices ===== | ||
- | The driver for the [[:ADP5520]] | + | * [[adi>ADP5520]] |
+ | * [[adi>ADP5501]] | ||
+ | ===== Evaluation Boards ===== | ||
+ | |||
+ | * [[adi> | ||
===== Description ===== | ===== Description ===== | ||
Line 355: | Line 359: | ||
</ | </ | ||
- | __**For more information on Input handling in Linux read:**__ [[git.linux.org> | + | __**For more information on Input handling in Linux read:**__ [[git.linux.org> |
+ | |||
+ | ====== More Information ====== | ||
+ | |||
+ | {{page> | ||