Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:linux-drivers:jesd204:axi_jesd204_rx [03 Jun 2019 14:27] – [Example platform device initialization] Michael Hennerichresources:tools-software:linux-drivers:jesd204:axi_jesd204_rx [15 Nov 2023 11:39] (current) – [Sysfs Interface] Michael Hennerich
Line 1: Line 1:
-====== ADI JESD204B Receive Peripheral Linux Driver ======+====== ADI JESD204B/C Receive Peripheral Linux Driver ======
  
 ===== Supported Devices ===== ===== Supported Devices =====
  
-  * [[resources:fpga:peripherals:jesd204:axi_jesd204_rx|ADI JESD204B Receive Peripheral]]+  * [[resources:fpga:peripherals:jesd204:axi_jesd204_rx|ADI JESD204B/C Receive Peripheral]]
  
 ===== Description ===== ===== Description =====
  
-The AXI JESD204B RX peripheral driver is a simple driver that supports the [[resources:fpga:peripherals:jesd204:axi_jesd204_tx|ADI JESD204B Receive Peripheral]]. The driver reads JESD204B link configuration data from the devicetree and configures the peripheral accordingly. After configuration has completed the JESD204B link is enabled. Link state can be monitored through sysfs files.+The AXI JESD204B RX peripheral driver is a simple driver that supports the [[resources:fpga:peripherals:jesd204:axi_jesd204_rx|ADI JESD204B Receive Peripheral]]. The driver reads JESD204B link configuration data from the devicetree and configures the peripheral accordingly. After configuration has completed the JESD204B link is enabled. Link state can be monitored through sysfs files.
  
 +This driver also work in conjunction with the [[resources:tools-software:linux-drivers:jesd204:jesd204-fsm-framework|JESD204 (FSM) Interface Linux Kernel Framework]], in this case JESD204B link configuration is provided by the JESD204-FSM framework. 
 ====== Source Code ====== ====== Source Code ======
  
Line 20: Line 21:
 | driver  | [[linux.github>master?drivers/iio/jesd204/axi_jesd204_rx.c | drivers/iio/jesd204/axi_jesd204_rx.c]] | | driver  | [[linux.github>master?drivers/iio/jesd204/axi_jesd204_rx.c | drivers/iio/jesd204/axi_jesd204_rx.c]] |
  
-====== Example platform device initialization ======+====== Example platform device / device tree initialization ======
  
 The AXI JESD204B driver is a platform driver and can currently only be instantiated via device tree. The AXI JESD204B driver is a platform driver and can currently only be instantiated via device tree.
  
 +===== Deprecated Non-jesd204-fsm mode =====
 + 
 Required devicetree properties: Required devicetree properties:
   * **compatible**: Must always be "adi,axi-jesd204-rx-1.00.a"   * **compatible**: Must always be "adi,axi-jesd204-rx-1.00.a"
Line 49: Line 52:
  adi,octets-per-frame = <32>;  adi,octets-per-frame = <32>;
  adi,frames-per-multiframe = <4>;  adi,frames-per-multiframe = <4>;
 + };
 +</code>
 +
 +===== jesd204-fsm mode =====
 +
 +When using the [[resources:tools-software:linux-drivers:jesd204:jesd204-fsm-framework|JESD204 (FSM) Interface Linux Kernel Framework]] the JESD link parameters are broadcasted by the framework to all link components.
 +
 +
 +Required devicetree properties:
 +  * **compatible**: Must always be "adi,axi-jesd204-rx-1.00.a"
 +  * **reg**: Base address and register area size. This parameter expects a register range.
 +  * **interrupts**: Property with a value describing the interrupt number.
 +  * **clock-names**: List of input clock names - "s_axi_aclk", "device_clk", "lane_clk"
 +  * **clocks**: Clock phandles and specifiers (See clock bindings for details on clock-names and clocks).
 +  * **jesd204-device**: Adds device to the jesd204-fsm kernel framework
 +  * **jesd204-inputs**: jesd204-fsm devices phandles and specifiers (used to build the link topology) 
 +
 +Optional devicetree clock-names:
 +  * **link_clk**: When using the link layer gearbox in order to support NP=12 modes, ''device_clk'' and ''link_clock'' need to be different. This is typical the case in case ''SYNTH_DATA_PATH_WIDTH'' and ''TPL_DATA_PATH_WIDTH'' differs. Then ''device_clk'' becomes ''link_clk'' times ''SYNTH_DATA_PATH_WIDTH'' / ''TPL_DATA_PATH_WIDTH''. ''link_clk'' still needs to be ''lane_clk'' / 40 for **JESD204B/8B10B** encoding and ''lane_clk'' / 66 for **JESD204C/64B66B** encoding.
 +  * **conv2**: Optional SERDES (CPLL/QPLL) REFCLK from a difference source which rate and state must be in sync with the main conv clk.
 +
 +
 +Example:
 +<code>
 + axi_ad9081_rx_jesd: axi-jesd204-rx@84a90000 {
 + compatible = "adi,axi-jesd204-rx-1.0";
 + reg = <0x84a90000 0x1000>;
 +
 + interrupts = <0 107 IRQ_TYPE_LEVEL_HIGH>;
 +
 + clocks = <&zynqmp_clk 71>, <&hmc7044 10>, <&axi_ad9081_adxcvr_rx 0>;
 + clock-names = "s_axi_aclk", "device_clk", "lane_clk";
 +
 + jesd204-device;
 + #jesd204-cells = <2>;
 + jesd204-inputs = <&axi_ad9081_adxcvr_rx 0 FRAMER_LINK0_RX>;
  };  };
 </code> </code>
Line 71: Line 110:
          [--snip--]          [--snip--]
 </code> </code>
 +
 +====== Sysfs Interface ======
 +
 +This driver provides advanced diagnostics, status and via [[wp>sysfs]]. A brief summary is with examples are provided below. 
 +
 +
 +<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap>
 +<xterm>
 +root@analog:/sys/bus/platform/devices/84a90000.axi-jesd204-rx# **ls -al**
 +total 0
 +drwxr-xr-x  4 root root    0 Feb  6 13:41 .
 +drwxr-xr-x 12 root root    0 Feb  6 13:41 ..
 +lrwxrwxrwx  1 root root    0 Feb  6 13:41 driver -> ../../../../bus/platform/drivers/axi-jesd204-rx
 +-rw-r--r--  1 root root 4096 Feb  6 16:27 driver_override
 +-r--r--r--  1 root root 4096 Feb  6 16:27 encoder
 +drwxr-xr-x  3 root root    0 Feb  6 13:41 jesd204:4
 +-r--------  1 root root 4096 Feb  6 16:27 lane0_info
 +-r--------  1 root root 4096 Feb  6 16:27 lane1_info
 +-r--------  1 root root 4096 Feb  6 16:27 lane2_info
 +-r--------  1 root root 4096 Feb  6 16:27 lane3_info
 +-r--------  1 root root 4096 Feb  6 16:27 lane4_info
 +-r--------  1 root root 4096 Feb  6 16:27 lane5_info
 +-r--------  1 root root 4096 Feb  6 16:27 lane6_info
 +-r--------  1 root root 4096 Feb  6 16:27 lane7_info
 +-r--r--r--  1 root root 4096 Feb  6 16:27 modalias
 +lrwxrwxrwx  1 root root    0 Feb  6 16:27 of_node -> ../../../../firmware/devicetree/base/fpga-axi@0/axi-jesd204-rx@84a90000
 +drwxr-xr-x  2 root root    0 Feb  6 16:27 power
 +-r--r--r--  1 root root 4096 Feb  6 16:27 status
 +lrwxrwxrwx  1 root root    0 Feb  6 13:41 subsystem -> ../../../../bus/platform
 +-rw-r--r--  1 root root 4096 Feb  6 13:41 uevent
 +</xterm></WRAP>
 +
 +**Reading the device/link status:**
 +
 +^ What ^ Comment ^
 +| Link is [enabled%%|%%disabled] | Link state indicator. In case link state is disabled, that either means the link was never enabled or that an error occurred and the FSM rolled back and disabled the link. In the jesd204-fsm case this can be prevented by using the ''jesd204-ignore-errors;'' devicetree property when placed in the jesd204-fsm jesd204-top-device node. |
 +| Link status | Depending on the encoding JESD204B/C 8B10B/64B66B there can be different values ''RESET'', ''WAIT'', ''CGS'', ''ILAS'', etc., ''DATA'' Please see link layer documentation for the state machine: [[resources:fpga:peripherals:jesd204:axi_jesd204_rx|JESD204B/C Link Receive Peripheral]] \ [[resources:fpga:peripherals:jesd204:axi_jesd204_tx|JESD204B/C Link Transmit Peripheral]] In general ''DATA'' is the desired state indicating proper operation. |
 +| SYNC is [asserted%%|%%deasserted] (8B10B only) | State of the external ''SYNC'' signal. |
 +| SYSREF captured: [Yes%%|%%No] (Subclass 1 only)  | Yes indicates that a ''SYSREF'' pulse was captured. |
 +| SYSREF alignment error: [Yes%%|%%No] (Subclass 1 only) | Yes indicates that a ''SYSREF'' event has been observed which was unaligned, in regards to the ''LMFC/LEMC'' period, to a previously recorded ''SYSREF'' event. |
 +| Lane rate  | The ''SERDES'' lane rate / bit clock. |  
 +| [LMFC%%|%%LEMC] rate | Frequency of the internal local multiframe clocks (''LMFC'')/ local-multiblock-clock (''LEMC''). |
 +| Lane rate / [40%%|%%66]  | Is equal to the desired ''Link Clock'' frequency. |
 +| Reported Link Clock | Is the ''Link Clock'' frequency which is reported by the common clock framework. If this rate is different from the desired ''Link Clock'' frequency, there is likely a problem. For example the clock provider wasn’t able to set the desired value. |   
 +| Measured Link Clock  | Is the measured ''Link Clock'', using a frequency counter inside the Link Layer Peripheral. For proper operation desired, reported and measured frequency must match. |
 +| Desired Device Clock | In case this value is different from the Desired ''Link Clock'', this indicates Dual Clock Operation required by the Gearbox. Please see Gearbox/Dual Clock Operation in the Link Layer Peripheral documentation: [[resources:fpga:peripherals:jesd204:axi_jesd204_rx|JESD204B/C Link Receive Peripheral]] \ [[resources:fpga:peripherals:jesd204:axi_jesd204_tx|JESD204B/C Link Transmit Peripheral]] The ''Device Clock'' is typically generated by the clock provider which also provides ''SYSREF''. |   
 +| Reported Device Clock | Is the ''Device Clock'' frequency which is reported by the common clock framework. If this rate is different from the desired ''Device Clock'' frequency, there is likely a problem. For example the clock provider wasn’t able to set the desired value. |   
 +| Measured Device Clock | Is the measured ''Device Clock'', using a frequency counter inside the Link Layer Peripheral. For proper operation desired, reported and measured frequency must match. |
 +
 +
 +<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap>
 +<xterm>
 +root@analog:/sys/bus/platform/devices/84a90000.axi-jesd204-rx# **cat status**
 +Link is enabled
 +Measured Link Clock: 375.034 MHz
 +Reported Link Clock: 375.000 MHz
 +Measured Device Clock: 375.034 MHz
 +Reported Device Clock: 375.000 MHz
 +Desired Device Clock: 375.000 MHz
 +Lane rate: 15000.000 MHz
 +Lane rate / 40: 375.000 MHz
 +LMFC rate: 46.875 MHz
 +Link status: DATA
 +SYSREF captured: Yes
 +SYSREF alignment error: No
 +</xterm></WRAP>
 +
 +**Reading the Encoder used:**
 +
 +<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap>
 +<xterm>
 +root@analog:/sys/bus/platform/devices/84a90000.axi-jesd204-rx# **cat encoder** 
 +8b10b
 +</xterm></WRAP>
 +
 +**Reading the Lane Status:**
 +
 +<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap>
 +<xterm>
 +root@analog:/sys/bus/platform/devices/84a90000.axi-jesd204-rx# **cat lane0_info** 
 +Errors: 0
 +CGS state: DATA
 +Initial Frame Synchronization: Yes
 +Lane Latency: 3 Multi-frames and 13 Octets
 +Initial Lane Alignment Sequence: Yes
 +DID: 0, BID: 0, LID: 2, L: 8, SCR: 1, F: 1
 +K: 32, M: 4, N: 16, CS: 0, N': 16, S: 1, HD: 0
 +FCHK: 0x9, CF: 0
 +ADJCNT: 0, PHADJ: 0, ADJDIR: 0, JESDV: 1, SUBCLASS: 1
 +FC: 15000000
 +</xterm></WRAP>
  
 ===== More Information ===== ===== More Information =====
  
   * [[resources:fpga:peripherals:jesd204|JESD204B High-Speed Serial Interface Support]]   * [[resources:fpga:peripherals:jesd204|JESD204B High-Speed Serial Interface Support]]
resources/tools-software/linux-drivers/jesd204/axi_jesd204_rx.txt · Last modified: 15 Nov 2023 11:39 by Michael Hennerich