Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:tools-software:linux-drivers:jesd204:axi_jesd204_rx [03 Jun 2019 14:27]
mhennerich [Example platform device initialization]
resources:tools-software:linux-drivers:jesd204:axi_jesd204_rx [31 Aug 2020 15:05]
mhennerich [Description]
Line 9: Line 9:
 The AXI JESD204B RX peripheral driver is a simple driver that supports the [[resources:​fpga:​peripherals:​jesd204:​axi_jesd204_tx|ADI JESD204B Receive Peripheral]]. The driver reads JESD204B link configuration data from the devicetree and configures the peripheral accordingly. After configuration has completed the JESD204B link is enabled. Link state can be monitored through sysfs files. The AXI JESD204B RX peripheral driver is a simple driver that supports the [[resources:​fpga:​peripherals:​jesd204:​axi_jesd204_tx|ADI JESD204B Receive Peripheral]]. The driver reads JESD204B link configuration data from the devicetree and configures the peripheral accordingly. After configuration has completed the JESD204B link is enabled. Link state can be monitored through sysfs files.
  
 +This driver also work in conjunction with the [[resources:​tools-software:​linux-drivers:​jesd204:​jesd204-fsm-framework|JESD204 (FSM) Interface Linux Kernel Framework]],​ in this case JESD204B link configuration is provided by the JESD204-FSM framework. ​
 ====== Source Code ====== ====== Source Code ======
  
resources/tools-software/linux-drivers/jesd204/axi_jesd204_rx.txt · Last modified: 31 Aug 2020 15:05 by mhennerich