This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:iio-transceiver:adrv9009 [11 Jan 2021 20:05] – remove wiki syntax in code block Robin Getz | resources:tools-software:linux-drivers:iio-transceiver:adrv9009 [12 Jul 2021 15:56] – [Channel Enable/Powerdown Controls] Michael Hennerich | ||
---|---|---|---|
Line 377: | Line 377: | ||
For use cases where pin control mode is not used or required, these attributes can be used to | For use cases where pin control mode is not used or required, these attributes can be used to | ||
enable/ | enable/ | ||
- | Rx and ORx channels **can not** be enabled at the same time, since they share the same converter. | + | |
+ | <note important> | ||
Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding channel powerdown option. | Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding channel powerdown option. |