This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:iio-transceiver:ad9371 [04 Feb 2021 20:14] – [PRBS] liam beguin | resources:tools-software:linux-drivers:iio-transceiver:ad9371 [28 Feb 2022 15:08] (current) – [Calibration Tracking Controls] Michael Hennerich | ||
---|---|---|---|
Line 86: | Line 86: | ||
| ADRV9371 Device Tree | [[linux.github> | | ADRV9371 Device Tree | [[linux.github> | ||
| ADRV9371 Device Tree | [[linux.github> | | ADRV9371 Device Tree | [[linux.github> | ||
+ | | ADRV9371 Device Tree | [[linux.github> | ||
| ADRV9375 Device Tree | [[linux.github> | | ADRV9375 Device Tree | [[linux.github> | ||
+ | |||
+ | |||
====== Enabling Linux driver support ====== | ====== Enabling Linux driver support ====== | ||
Line 687: | Line 690: | ||
root:/ | root:/ | ||
0 | 0 | ||
+ | </ | ||
+ | |||
+ | ===== ARM Calibrations | ||
+ | |||
+ | Sometimes a certain calibration is not required during power-up, or some other external condition must be met. The attributes detailed below allow the user to reschedule a calibration. | ||
+ | |||
+ | Writing 0, N or 1, Y to the below attributes either disables or enables the corresponding init calibration. They are not run immediately, | ||
+ | |||
+ | * calibrate_rx_qec_en | ||
+ | * calibrate_tx_lol_en | ||
+ | * calibrate_tx_lol_ext_en | ||
+ | * calibrate_tx_qec_en | ||
+ | * calibrate | ||
+ | |||
+ | |||
+ | <WRAP box bggreen>< | ||
+ | < | ||
+ | root:/ | ||
+ | 0 | ||
+ | root:/ | ||
+ | root:/ | ||
+ | 1 | ||
+ | root:/ | ||
</ | </ | ||