This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:iio-resolver:ad2s1200 [09 Sep 2011 16:04] – [Adding Linux driver support] Michael Hennerich | resources:tools-software:linux-drivers:iio-resolver:ad2s1200 [20 Nov 2015 16:33] (current) – [Description] Lars-Peter Clausen | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== Supported Devices ===== | ===== Supported Devices ===== | ||
- | This driver supports the\\ | + | * [[adi> |
- | [[adi> | + | |
- | [[adi> | + | |
+ | ===== Evaluation Boards ===== | ||
- | ===== Description ===== | + | * [[adi> |
+ | * [[adi> | ||
- | {{scrape> | + | ===== Description ===== |
* [[adi> | * [[adi> | ||
- | * {{scrape> | ||
This is a Linux industrial I/O ([[software: | This is a Linux industrial I/O ([[software: | ||
Line 22: | Line 23: | ||
===== Status ===== | ===== Status ===== | ||
- | ^ Source | + | ^ Source ^ Mainlined? ^ |
- | | [[bfgit>linux-kernel?drivers/ | + | | [[git.linux.org>drivers/ |
===== Files ===== | ===== Files ===== | ||
^ Function ^ File ^ | ^ Function ^ File ^ | ||
- | | driver | + | | driver | [[staging.kernel.org> |
====== Adding Linux driver support ====== | ====== Adding Linux driver support ====== | ||
Line 35: | Line 36: | ||
"make qconfig" | "make qconfig" | ||
- | <note> | + | <WRAP round help> |
The Driver depends on **CONFIG_SPI** | The Driver depends on **CONFIG_SPI** | ||
- | </note> | + | </WRAP> |
< | < |