This is an old revision of the document!
HMC7044 Clock Jitter Attenuator with JESD204B Linux Driver
Supported Devices
Description
HMC7044 is a high performance, dual-loop, integer-N jitter attenuator capable of performing reference selection and generation of ultralow phase noise frequencies for high speed data converters with either parallel or serial (JESD204B type) interfaces.
This is a Linux industrial I/O (IIO) subsystem driver, targeting serial interface PLL Synthesizers.
The industrial I/O subsystem provides a unified framework for drivers for many different types of converters and sensors using a number of different physical interfaces (i2c, spi, etc).
See IIO for more information.
Source Code
Status
Files
Enabling the driver
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or
“make qconfig”)
The HMC7044 Driver depends on CONFIG_SPI
Linux Kernel Configuration
Device Drivers --->
<*> Industrial I/O support --->
Frequency Synthesizers DDS/PLL --->
Clock Generator/Distribution --->
<*> Analog Devices HMC7044 Clock Jitter Attenuator with JESD204B
Adding a device tree entry
Available properties
Required properties:
compatible: Should be “adi,hmc7044”.
reg:
SPI chip select number.
spi-max-frequency: Max
SPI frequency to use (⇐ 10000000).
adi,pll1-clkin-frequencies: An array of 4 elements, each representing the frequency of CLKINx PLL1 reference input (CLKIN0, CLKIN1, CLKIN2, CLKIN3).
adi,vcxo-frequency: The frequency of the VCXO.
adi,pll2-output-frequency: The desired output frequency of the PLL2.
adi,gpi-controls: An array of 4 elements (each corresponding to GPI1, GPI2, GPI3 and GPI4, respectively), representing the GPI selection (Bits [4:1]) and the GPI enable bit ([0]) - see registers 0x0046, 0x0047, 0x0048, 0x0049.
adi,gpo-controls: An array of 4 elements (each corresponding to GPO1, GPO2, GPO3 and GPO4, respectively), representing the GPO selection (Bits [7:2]), the GPO mode (Bit [1]) and the GPO enable bit ([0]) - see registers 0x0050, 0x0051, 0x0052, 0x0053.
clock-output-names: An array of 14 elements, representing the names of the output clocks.
Optional properties:
adi,pll1-loop-bandwidth-hz: The PLL1 loop bandwidth. If this is not specified, 200 will be used by default.
adi,sysref-timer-divider: This sets the internal beat frequency of the master timer, which controls synchronization and pulse generator events. It should be set to a submultiple of the lowest output SYSREF frequency, no faster than 4
MHz. If this is not specified, 1024 will be used by default.
adi,pulse-generator-mode: Pulse Generator Mode Selection [Bits 2:0] - see register 0x005A. If this is not specified, 0 will be used by default.
adi,clkin0-buffer-mode: CLKIN0 Input Buffer Control, for specifying the Input Buffer Mode (Bits [4:1]) and the Buffer enable bit ([0]) - see register 0x000A. If this is not specified, 0 will be used by default.
adi,clkin1-buffer-mode: CLKIN1 Input Buffer Control, for specifying the Input Buffer Mode (Bits [4:1]) and the Buffer enable bit ([0]) - see register 0x000B. If this is not specified, 0 will be used by default.
adi,clkin2-buffer-mode: CLKIN2 Input Buffer Control, for specifying the Input Buffer Mode (Bits [4:1]) and the Buffer enable bit ([0]) - see register 0x000C. If this is not specified, 0 will be used by default.
adi,clkin3-buffer-mode: CLKIN3 Input Buffer Control, for specifying the Input Buffer Mode (Bits [4:1]) and the Buffer enable bit ([0]) - see register 0x000D. If this is not specified, 0 will be used by default.
adi,oscin-buffer-mode: OSCIN Input Buffer Control, for specifying the Input Buffer Mode (Bits [4:1]) and the Buffer enable bit ([0]) - see register 0x000E. If this is not specified, 0 will be used by default.
Adding channels
Channels can be specified using child nodes. The following properties are applicable to them:
reg: The identifier of the channel.
adi,extended-name: Descriptive channel name.
adi,divider: Channel divider. The divider supports even divide ratios from 2 to 4094. The supported odd divide ratios are 1, 3, and 5.
adi,driver-mode: Output driver mode. Must be one of:
0 - CML mode,
1 - LVPECL mode,
2 - LVDS mode,
3 - CMOS mode.
adi,high-performance-mode-disable:Disables the high performance mode
adi,startup-mode-dynamic-enable:Enables pulse generator mode (default mode is asynchronous)
adi,force-mute-enable: When not generating pulses in dynamic mode the output is forced to logic-0
adi,coarse-digital-delay: Adjusts the phase of the divider signal by up to 17 1/2 cycles of the VCO
adi,fine-analog-delay: Adjusts the delay of the divider signal in 24 fine delay steps. Step size = 25 ps.
adi,output-mux-mode: Configures the output mux selection:
Device tree example
The following example instanciates the hmc7044 driver for a HMC7044 device connected on the SPI bus to the chip-select line 0.
hmc7044: hmc7044@0 {
compatible = "adi,hmc7044";
reg = <0>;
spi-max-frequency = <10000000>;
adi,pll1-clkin-frequencies = <122880000 0 0 0>;
adi,pll1-loop-bandwidth = <200>;
adi,vcxo-frequency = <122880000>;
adi,pll2-output-frequency = <2949120000>;
adi,sysref-timer-divider = <1024>;
adi,pulse-generator-mode = <0>;
adi,clkin0-buffer-mode = <0x15>;
adi,oscin-buffer-mode = <0x15>;
adi,gpi-controls = <0x00 0x00 0x00 0x00>;
adi,gpo-controls = <0x1f 0x2b 0x00 0x00>;
clock-output-names = "hmc7044_out0", "hmc7044_out1", "hmc7044_out2",
"hmc7044_out3", "hmc7044_out4", "hmc7044_out5",
"hmc7044_out6", "hmc7044_out7", "hmc7044_out8",
"hmc7044_out9", "hmc7044_out10", "hmc7044_out11",
"hmc7044_out12", "hmc7044_out13";
hmc7044_c2: channel@2 {
reg = <2>;
adi,extended-name = "DAC_CLK";
adi,divider = <1>;
adi,driver-mode = <1>;
};
hmc7044_c3: channel@3 {
reg = <3>;
adi,extended-name = "DAC_SYSREF";
adi,divider = <512>;
adi,driver-mode = <1>;
};
hmc7044_c12: channel@12 {
reg = <12>;
adi,extended-name = "FPGA_CLK";
adi,divider = <8>;
adi,driver-mode = <2>;
};
hmc7044_c13: channel@13 {
reg = <13>;
adi,extended-name = "FPGA_SYSREF";
adi,divider = <512>;
adi,driver-mode = <2>;
};
};