This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-drivers:iio-pll:ad9523 [20 Nov 2012 10:42] – [Evaluation Boards] Lars-Peter Clausen | resources:tools-software:linux-drivers:iio-pll:ad9523 [03 Jan 2013 20:42] – external edit | ||
---|---|---|---|
Line 325: | Line 325: | ||
"make qconfig" | "make qconfig" | ||
- | <note> | + | <WRAP round help> |
The AD9523 Driver depends on **CONFIG_SPI** | The AD9523 Driver depends on **CONFIG_SPI** | ||
- | </note> | + | </WRAP> |
< | < | ||
Line 352: | Line 352: | ||
{{page> | {{page> | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cd / | root:/> **cd / | ||
Line 401: | Line 401: | ||
-rw-r--r-- | -rw-r--r-- | ||
-r--r--r-- | -r--r--r-- | ||
- | </ | + | </ |
=== Show device name === | === Show device name === | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cd / | root:/> **cd / | ||
root:/> **cat name** | root:/> **cat name** | ||
ad9523-lpc | ad9523-lpc | ||
- | </ | + | </ |
=== Set ChannelY Output Frequency === | === Set ChannelY Output Frequency === | ||
Line 421: | Line 421: | ||
channel. | channel. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cat out_altvoltage1_DAC_CLK_frequency** | root:/> **cat out_altvoltage1_DAC_CLK_frequency** | ||
Line 428: | Line 428: | ||
root:/> **cat out_altvoltage1_DAC_CLK_frequency** | root:/> **cat out_altvoltage1_DAC_CLK_frequency** | ||
245760000 | 245760000 | ||
- | </ | + | </ |
=== Set ChannelY Output Divider Phase === | === Set ChannelY Output Divider Phase === | ||
Line 440: | Line 440: | ||
channel. | channel. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cat out_altvoltage1_DAC_CLK_phase** | root:/> **cat out_altvoltage1_DAC_CLK_phase** | ||
Line 447: | Line 447: | ||
root:/> **cat out_altvoltage1_DAC_CLK_phase** | root:/> **cat out_altvoltage1_DAC_CLK_phase** | ||
3.1415920 | 3.1415920 | ||
- | </ | + | </ |
=== Disable / Power Down ChannelY === | === Disable / Power Down ChannelY === | ||
Line 456: | Line 456: | ||
any value > 0 enables the channel. | any value > 0 enables the channel. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cat out_altvoltage1_DAC_CLK_raw** | root:/> **cat out_altvoltage1_DAC_CLK_raw** | ||
Line 463: | Line 463: | ||
root:/> **cat out_altvoltage1_DAC_CLK_raw** | root:/> **cat out_altvoltage1_DAC_CLK_raw** | ||
0 | 0 | ||
- | </ | + | </ |
=== Query Device Status === | === Query Device Status === | ||
Line 480: | Line 480: | ||
means that the clock is missing or the pllY is unlocked. | means that the clock is missing or the pllY is unlocked. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cat pll1_locked** | root:/> **cat pll1_locked** | ||
Line 495: | Line 495: | ||
vcxo_clk_present: | vcxo_clk_present: | ||
- | </ | + | </ |
=== Save Current Device Config to EEPROM === | === Save Current Device Config to EEPROM === | ||
Line 505: | Line 505: | ||
automatically load the saved configuration. | automatically load the saved configuration. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **echo 1 > store_eeprom** | root:/> **echo 1 > store_eeprom** | ||
- | </ | + | </ |
=== SYNC Device === | === SYNC Device === | ||
Line 520: | Line 520: | ||
/SYNC pin low. | /SYNC pin low. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **echo 1 > sync_dividers** | root:/> **echo 1 > sync_dividers** | ||
- | </ | + | </ |
====== More Information ====== | ====== More Information ====== | ||
{{page> | {{page> |