Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:tools-software:linux-drivers:iio-dds:axi-dac-dds-hdl [12 Apr 2019 10:37] – [Supported Boards] Michael Hennerich | resources:tools-software:linux-drivers:iio-dds:axi-dac-dds-hdl [22 Nov 2023 10:08] (current) – Add support for AD9783 iulia Moldovan |
---|
===== Supported Devices ===== | ===== Supported Devices ===== |
* [[adi>AD9122]] | * [[adi>AD9122]] |
| * [[adi>AD9136]] |
* [[adi>AD9144]] | * [[adi>AD9144]] |
* [[adi>AD9152]] | * [[adi>AD9152]] |
| * [[adi>AD9154]] |
* [[adi>AD9162]] | * [[adi>AD9162]] |
* [[adi>AD9171]] | * [[adi>AD9171]] |
* [[adi>AD9371]] | * [[adi>AD9371]] |
* [[adi>AD9739A]] | * [[adi>AD9739A]] |
| * [[adi>AD9783]] |
| |
===== Supported Boards ===== | ===== Supported Boards ===== |
This driver supports the\\ | This driver supports the\\ |
* [[resources/eval/user-guides/ad-fmcomms1-ebz |AD-FMCOMMS1-EBZ FMC Card]] | * [[resources/eval/user-guides/ad-fmcomms1-ebz |AD-FMCOMMS1-EBZ FMC Card]] |
* [[resources/eval/user-guides/ad-fmcomms3-ebz |AD-FMCOMMS3-EBZ FMC Card]] | * [[resources/eval/user-guides/ad-fmcomms3-ebz |AD-FMCOMMS3-EBZ FMC Card]] |
* [[resources/eval/user-guides/ad-fmcomms4-ebz |AD-FMCOMMS4-EBZ FMC Card]] | * [[resources/eval/user-guides/ad-fmcomms4-ebz |AD-FMCOMMS4-EBZ FMC Card]] |
* [[resources/eval/user-guides/ad-fmcomms5-ebz |AD-FMCOMMS5-EBZ FMC Card]] | * [[resources/eval/user-guides/ad-fmcomms5-ebz |AD-FMCOMMS5-EBZ FMC Card]] |
| * [[resources:eval:user-guides:ad-fmcomms11-ebz|AD-FMCOMMS11-EBZ User Guide]] |
* [[resources/eval/user-guides/ad-fmcdaq2-ebz|AD-FMCDAQ2-EBZ FMC Card]] | * [[resources/eval/user-guides/ad-fmcdaq2-ebz|AD-FMCDAQ2-EBZ FMC Card]] |
| * [[resources:eval:user-guides:ad-fmcdaq3-ebz|AD-FMCDAQ3-EBZ User Guide]] |
* [[resources/fpga/xilinx/fmc/ad9739a | AD9739A Native FMC Card / Xilinx Reference Designs]] | * [[resources/fpga/xilinx/fmc/ad9739a | AD9739A Native FMC Card / Xilinx Reference Designs]] |
* [[resources/fpga/xilinx/interposer/ad9739a | AD9739A Evaluation Board, DAC-FMC Interposer & Xilinx Reference Design]] | * [[resources/fpga/xilinx/interposer/ad9739a | AD9739A Evaluation Board, DAC-FMC Interposer & Xilinx Reference Design]] |
| * [[:resources:eval:dpg:eval-ad9783 | EVALUATING THE AD9780/AD9781/AD9783 DIGITAL-TO-ANALOG CONVERTERS]] |
| * [[:resources:fpga:xilinx:interposer:ad9783 | AD9783 Evaluation Board, DAC-FMC Interposer & Xilinx Reference Design]] |
* [[resources/eval/user-guides/mykonos | ADRV9371 FMC Card]] | * [[resources/eval/user-guides/mykonos | ADRV9371 FMC Card]] |
| * [[resources:eval:user-guides:adrv9009|ADRV9009 & ADRV9008 Prototyping Platform User Guide]] |
* [[resources:eval:dpg:eval-ad9172|AD9171/AD9172/AD9173/AD9174/AD9175/AD9176 Evaluation Board]] | * [[resources:eval:dpg:eval-ad9172|AD9171/AD9172/AD9173/AD9174/AD9175/AD9176 Evaluation Board]] |
| |
| ===== Supported HDL Cores ===== |
| |
| * [[resources:fpga:docs:axi_dac_ip|Generic AXI DAC]] |
| * [[resources:fpga:peripherals:jesd204:jesd204_tpl_dac|DAC JESD204B Transport Peripheral]] |
| * [[resources:fpga:docs:axi_ad9144|AXI_AD9144]] |
| * [[resources:fpga:docs:axi_ad9361|AXI_AD9361]] |
| * [[resources:fpga:docs:axi_ad9371|AXI_AD9371]] |
| * [[:resources:fpga:docs:axi_ad9783|AXI_AD9783]] |
| |
| ===== Sub device Documentation (linked mode) ===== |
| |
| * [[resources:tools-software:linux-drivers:iio-dds:ad9172|AD9172 DAC Linux Driver]] |
===== Description ===== | ===== Description ===== |
| |
The AXI DAC DDS HDL driver is the driver for the HDL interface core which is used on various FPGA designs. The driver is implemented as an Linux IIO driver. It's register map can be found here: [[resources:fpga:docs:hdl:regmap|Base register map (common to all cores)]] | The AXI DAC DDS HDL driver is the driver for various HDL interface cores which are used on different FPGA designs. The driver is implemented as an Linux IIO driver. It's register map can be found here: [[resources:fpga:docs:hdl:regmap|Base register map (common to all cores)]] |
| |
| This driver is independent from the physical layer. So it's being used with CMOS or LVDS type interfaces or the [[resources:fpga:peripherals:jesd204|JESD204 Interface Framework]]. |
| |
| There are basically two use case scenarios for this driver, in which this driver controls only the HDL/FPGA transport layer capture core. This mode is called ''standalone mode'', and the converter is fully configured and controlled by a separate driver. |
| The Linux common clock framework is utilized so that this driver knows the sampling frequency of the connected converter DAC device. |
| Alternatively this driver can also be used in a ''linked mode'', where the converter device typically a SPI device must instantiate first. If this has happened this AXI-DAC driver will then probe as well. (Deferred probe mechanism) |
| Finally both the HDL core platform device together with the converter SPI device will register a common IIO device, which will then exhibit a common set of attributes and channels. |
| The converter SPI device driver is handled in a separate source file, which can be found in the same directory this driver exists. The device tree phandle “spibus-connected” is used to connect the AXI-DAC driver with the SPI control driver. |
| |
| Sometimes there is a common HDL/FPGA transport layer core, which handles both RX/TX or ADC/DMA. |
| This single physical core is then handled by two independent IIO drivers each for one transport data direction. |
| It’s physical address register space is then also split or divided, typically spaced by 0x4000. |
| A good example for this case is the [[resources:fpga:docs:axi_ad9361|AXI_AD9361]] HDL core. |
| |
| |
| The HDL/FPGA transport layer capture core driver portion implements a polyphase dual tone DDS core per channel together with an DMA based waveform buffer mechanism. |
| The buffer can be filled by arbitrary data, which is then typically cyclically repeated or used in a streaming fashion. |
| |
This driver implements a polyphase dual tone DDS core per channel together with an waveform buffer mechanism. | |
The buffer can be filled by arbitrary data, which is then typically cyclically repeated. | |
| |
{{ :resources:tools-software:linux-drivers:iio-dds:axi-dac-dds-overview.png?800 |}} | {{ :resources:tools-software:linux-drivers:iio-dds:axi-dac-dds-overview.png?800 |}} |
| |
^ Source ^ Mainlined? ^ | ^ Source ^ Mainlined? ^ |
| [[linux.github>master?drivers/iio/frequency/cf_axi_dds.c | drivers/iio/frequency/cf_axi_adc_core.c]] | [[git.linux.org>drivers/iio/frequency/cf_axi_dds.c|WIP]] | | | [[linux.github>master?drivers/iio/frequency/cf_axi_dds.c | drivers/iio/frequency/cf_axi_dds.c]] | [[git.linux.org>drivers/iio/frequency/cf_axi_dds.c|WIP]] | |
| |
===== Files ===== | ===== Files ===== |
| driver | [[linux.github>master?drivers/iio/frequency/ad9122.c | drivers/iio/frequency/ad9122.c ]] | | | driver | [[linux.github>master?drivers/iio/frequency/ad9122.c | drivers/iio/frequency/ad9122.c ]] | |
| driver | [[linux.github>master?drivers/iio/frequency/ad9144.c | drivers/iio/frequency/ad9144.c]] | | | driver | [[linux.github>master?drivers/iio/frequency/ad9144.c | drivers/iio/frequency/ad9144.c]] | |
| | driver | [[linux.github>master?drivers/iio/frequency/ad9162.c | drivers/iio/frequency/ad9162.c ]] | |
| | driver | [[linux.github>master?drivers/iio/frequency/ad9172.c | drivers/iio/frequency/ad9172.c]] | |
| driver | [[linux.github>master?drivers/iio/frequency/cf_axi_dds.c | drivers/iio/frequency/cf_axi_dds.c]] | | | driver | [[linux.github>master?drivers/iio/frequency/cf_axi_dds.c | drivers/iio/frequency/cf_axi_dds.c]] | |
| driver | [[linux.github>master?drivers/iio/frequency/cf_axi_dds_buffer_stream.c | drivers/iio/frequency/cf_axi_dds_buffer_stream.c ]] | | | driver | [[linux.github>master?drivers/iio/frequency/cf_axi_dds_buffer_stream.c | drivers/iio/frequency/cf_axi_dds_buffer_stream.c ]] | |
* **compatible**: Should always be one of these: | * **compatible**: Should always be one of these: |
* adi,axi-ad9122-6.00.a | * adi,axi-ad9122-6.00.a |
| * adi,axi-ad9136-1.0 |
* adi,axi-ad9144-1.0 | * adi,axi-ad9144-1.0 |
* adi,axi-ad9739a-8.00.b | * adi,axi-ad9162-1.0 |
| * adi,axi-ad9172-1.0 |
* adi,axi-ad9361x2-dds-6.00.a | * adi,axi-ad9361x2-dds-6.00.a |
* adi,axi-ad9361-dds-6.00.a | * adi,axi-ad9361-dds-6.00.a |
* adi,axi-ad9364-dds-6.00.a | * adi,axi-ad9364-dds-6.00.a |
* adi,axi-ad9371-tx-1.0 | * adi,axi-ad9371-tx-1.0 |
* adi,axi-ad9162-1.0 | * adi,axi-ad9739a-8.00.b |
| * adi,axi-ad9963-dds-1.00.a |
| * adi,axi-adrv9009-tx-1.0 |
| |
* **reg**: Base address and register area size. This parameter expects a register range. | * **reg**: Base address and register area size. This parameter expects a register range. |
| |
</xterm></WRAP> | </xterm></WRAP> |
| |
| === External synchronization === |
| |
| The [[resources:fpga:peripherals:jesd204:jesd204_tpl_dac|DAC TPL HDL]] core supports the [[resources:fpga:peripherals:jesd204:jesd204_tpl_dac#External_synchronization|EXT_SYNC]] feature, allowing to synchronize multiple channels within a DAC or across multiple instances. |
| This feature can also synchronize between the [[resources:fpga:peripherals:jesd204:jesd204_tpl_adc|ADC TPL HDL]] and [[resources:fpga:peripherals:jesd204:jesd204_tpl_dac|DAC TPL HDL]] core. |
| |
| There are two device attributes which allows controlling this feature: |
| ''sync_start_enable'' and ''sync_start_enable_available'' reading the |
| later returns the available modes which depend on HDL core synthesis |
| parameters. The options are explained below. Reading 'sync_start_enable' |
| returns either 'arm' while waiting for the external synchronization |
| signal or 'disarm' otherwise. |
| |
| * ''arm'': Setting this key will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a DAC, and across multiple instances. This key has an effect only the EXT_SYNC synthesis parameter is set. |
| |
| * ''disarm'': Setting this key will disarm the trigger mechanism sensitive to an external sync signal. This key has an effect only the EXT_SYNC synthesis parameter is set. |
| |
| * ''trigger_manual'': Setting this key will issue an external sync event if it is hooked up inside the fabric. This key has an effect only the EXT_SYNC synthesis parameter is set. |
| |
| == Example: == |
| |
| <WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> |
| <xterm> |
| root@analog:/sys/bus/iio/devices/iio:device3# **cat sync_start_enable_available** |
| **arm disarm trigger_manual** |
| root@analog:/sys/bus/iio/devices/iio:device3# **cat sync_start_enable** |
| **disarm** |
| root@analog:/sys/bus/iio/devices/iio:device3# **echo arm > sync_start_enable** |
| root@analog:/sys/bus/iio/devices/iio:device3# **cat sync_start_enable** |
| **arm** |
| root@analog:/sys/bus/iio/devices/iio:device3# **echo trigger_manual > sync_start_enable** |
| root@analog:/sys/bus/iio/devices/iio:device3# **cat sync_start_enable** |
| **disarm** |
| </xterm></WRAP> |
| |
| |
===== Buffer management ===== | ===== Buffer management ===== |
| |