This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:linux-drivers:iio-dac:ad5764 [05 Sep 2012 13:36] – fix out of staging links Michael Hennerich | resources:tools-software:linux-drivers:iio-dac:ad5764 [05 Jan 2021 16:01] (current) – Removed old references Ioana Chelaru | ||
---|---|---|---|
Line 8: | Line 8: | ||
* [[adi> | * [[adi> | ||
- | ===== Reference Circuits ===== | ||
- | |||
- | * [[adi> | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
Line 27: | Line 24: | ||
===== Status ===== | ===== Status ===== | ||
- | ^ Source | + | ^ Source ^ Mainlined? ^ |
| [[git.linux.org> | | [[git.linux.org> | ||
Line 141: | Line 138: | ||
"make qconfig" | "make qconfig" | ||
- | <note> | + | <WRAP round help> |
The AD5764 Driver depends on **CONFIG_SPI_MASTER** | The AD5764 Driver depends on **CONFIG_SPI_MASTER** | ||
- | </note> | + | </WRAP> |
< | < | ||
Linux Kernel Configuration | Linux Kernel Configuration | ||
- | Device Drivers | + | |
- | [*] Staging drivers | + | ... |
- | < | + | < |
- | | + | --- Industrial I/O support |
- | -*- | + | ... |
- | -*- | + | Digital to analog |
- | -*- | + | ... |
- | + | < | |
- | *** Digital to analog | + | ... |
- | [--snip--] | + | ... |
- | + | ... | |
- | | + | |
- | + | ||
- | [--snip--] | + | |
</ | </ | ||
- | |||
====== Hardware configuration ====== | ====== Hardware configuration ====== | ||
Line 171: | Line 164: | ||
{{page> | {{page> | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/> **cd / | root:/> **cd / | ||
Line 203: | Line 196: | ||
-rw-r--r-- | -rw-r--r-- | ||
- | </ | + | </ |
=== Show device name === | === Show device name === | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/ | root:/ | ||
ad5764 | ad5764 | ||
- | </ | + | </ |
=== Show scale === | === Show scale === | ||
Line 219: | Line 212: | ||
scale to be applied to out_voltageY_raw in order to obtain the measured voltage in millivolts. | scale to be applied to out_voltageY_raw in order to obtain the measured voltage in millivolts. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/ | root:/ | ||
0.305170 | 0.305170 | ||
- | </ | + | </ |
=== Show offset === | === Show offset === | ||
Line 232: | Line 225: | ||
The offset is applied before scale is applied. | The offset is applied before scale is applied. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/ | root:/ | ||
-32768 | -32768 | ||
- | </ | + | </ |
=== Set channel Y output voltage === | === Set channel Y output voltage === | ||
Line 246: | Line 239: | ||
channel Y. | channel Y. | ||
- | < | + | <WRAP box bggreen>< |
< | < | ||
root:/ | root:/ | ||
- | </ | + | </ |
**U** = // | **U** = // |