Wiki

This version (19 Jan 2018 10:13) was approved by Alexandru Ardelean.The Previously approved version (05 Dec 2017 14:11) is available.Diff

AD5593R IIO DAC/ADC Linux Driver

Supported Devices

Reference Circuits

Evaluation Boards

Description

The AD5593R have eight I/Ox pins (I/O0 to I/O7) that can be independently configured as digital-to-analog converter (DAC) outputs, analog-to-digital converter (ADC) inputs, digital outputs, or digital inputs. When an I/Ox pin is configured as an analog output, it is driven by a 12-bit DAC. The output range of the DAC is 0 V to VREF or 0 V to 2 × VREF. When an I/Ox pin is configured as an analog input, it is connected to a 12-bit ADC via an analog multiplexer. The input range of the ADC is 0 V to VREF or 0 V to 2 × VREF. The ADC has a total throughput rate of 400 kSPS. The I/Ox pins can also be configured as digital, general-purpose input or output (GPIO) pins. The state of the GPIO pins can be set or read back by accessing the GPIO write data register or the GPIO read configuration register, respectively, via an I2C write or read operation. The AD5593R have an integrated 2.5 V, 25 ppm/°C reference, which is turned off by default, and an integrated temperature indicator, which gives an indication of the die temperature. The temperature value is read back as part of an ADC read sequence.

Source Code

Status

Source Mainlined?
git Yes

Files

Hardware configuration

ad5592r_eval.jpg

Adding Linux driver support

Enabling the driver

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

The AD5593R Driver depends on CONFIG_I2C

Linux Kernel Configuration
    Device Drivers  --->
        ...
        <*>     Industrial I/O support --->
            --- Industrial I/O support
            ...
            Digital to analog converters  ---> 
                ...
                <*>   Analog Devices AD5593R ADC/DAC driver
                ...
            ...
        ...

Adding a device tree entry

Required properties

  • compatible: Must be one of:
    • “adi,ad5593r”
  • reg: I2C address of the chip (generally 0x10).
  • #address-cells: Should be 1.
  • #size-cells: Should be 0.
  • channel nodes:
    • Each child node represents one channel and has the following
    • Required properties:
    • reg: Pin on which this channel is connected to.
    • adi,mode: Mode or function of this channel. Macros specifying the valid values can be found in <dt-bindings/iio/adi,ad5592r.h>. The following values are currently supported:
      • CH_MODE_UNUSED (the pin is unused)
      • CH_MODE_ADC (the pin is ADC input)
      • CH_MODE_DAC (the pin is DAC output)
      • CH_MODE_DAC_AND_ADC (the pin is DAC output but can be monitored by an ADC, since there is no disadvantage this this should be considered as the preferred DAC mode)
      • CH_MODE_GPIO (the pin is registered with GPIOLIB)
  • Optional properties:
  • adi,off-state: State of this channel when unused or the device is removed. Macros specifying the valid values can be found in <dt-bindings/iio/adi,ad5592r.h>.
    • CH_OFFSTATE_PULLDOWN (the pin is pulled down)
    • CH_OFFSTATE_OUT_LOW (the pin is output low)
    • CH_OFFSTATE_OUT_HIGH (the pin is output high)
    • CH_OFFSTATE_OUT_TRISTATE (the pin is tristated output)

Optional properties

  • vref-supply: Phandle to the external reference voltage supply. This should only be set if there is an external reference voltage connected to the VREF pin. If the property is not set the internal 2.5V reference is used.
  • reset-gpios : GPIO spec for the RESET pin. If specified, it will be asserted during driver probe.
  • gpio-controller: Marks the device node as a GPIO controller.
  • #gpio-cells: Should be 2. The first cell is the GPIO number and the second cell specifies GPIO flags, as defined in <dt-bindings/gpio/gpio.h>.

Device tree example

The following example instanciates the ad5593r driver for a AD5593R device connected on a I2C bus. It sets the I/O0 port as a DAC, the I/O1 port as ADC. I/O2 and I/O3 are configured for primary function DAC the additional ADC can measure the voltage being provided by the DAC. This feature can monitor the output voltage to detect short circuits or overload conditions. I/O4 is connected to the ground with a pull-down resistor. The other I/Os are registered with the Linux GPIO subsystem.

	#include <dt-bindings/iio/adi,ad5592r.h>

	vref: regulator-vref {
		compatible = "regulator-fixed";
		regulator-name = "vref-ad559x";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		regulator-always-on;
	};

&i2c0 {
	status = "okay";
	clock-frequency = <400000>;
	ad5593r@10 {
		#size-cells = <0>;
		#address-cells = <1>;
		#gpio-cells = <2>;
		compatible = "adi,ad5593r";
		reg = <0x10>;
		gpio-controller;

		channel@0 {
			reg = <0>;
			adi,mode = <CH_MODE_DAC>;
			adi,off-state = <CH_OFFSTATE_PULLDOWN>;
		};
		channel@1 {
			reg = <1>;
			adi,mode = <CH_MODE_ADC>;
			adi,off-state = <CH_OFFSTATE_PULLDOWN>;
		};
		channel@2 {
			reg = <2>;
			adi,mode = <CH_MODE_DAC_AND_ADC>;
			adi,off-state = <CH_OFFSTATE_PULLDOWN>;
		};
		channel@6 {
			reg = <6>;
			adi,mode = <CH_MODE_GPIO>;
			adi,off-state = <CH_OFFSTATE_PULLDOWN>;
		};

		vref-supply = <&vref>; /* optional */
		reset-gpios = <&gpio0 86 0>;  /* optional */

	};

};

Driver testing

If the driver correctly detected the device, the “iio_info” program should inform us about the available channels:

root@linaro-ubuntu-desktop:~# iio_info 
IIO context created: local
IIO context has 3 devices:
        iio:device2: ad5593r
                7 channels found:
                        voltage0:  (output)
                        3 channel-specific attributes found:
                                attr 0: raw value: 0
                                attr 1: scale_available value: 0.732421875 1.464843750
                                attr 2: scale value: 0.732421875
                        voltage2:  (output)
                        3 channel-specific attributes found:
                                attr 0: raw value: 0
                                attr 1: scale_available value: 0.732421875 1.464843750
                                attr 2: scale value: 0.732421875
                        voltage3:  (output)
                        3 channel-specific attributes found:
                                attr 0: raw value: 0
                                attr 1: scale_available value: 0.732421875 1.464843750
                                attr 2: scale value: 0.732421875
                        voltage1:  (input)
                        3 channel-specific attributes found:
                                attr 0: raw value: 0
                                attr 1: scale value: 0.732421875
                                attr 2: scale_available value: 0.732421875 1.464843750
                        voltage2:  (input)
                        3 channel-specific attributes found:
                                attr 0: raw value: 1
                                attr 1: scale value: 0.732421875
                                attr 2: scale_available value: 0.732421875 1.464843750
                        voltage3:  (input)
                        3 channel-specific attributes found:
                                attr 0: raw value: 0
                                attr 1: scale value: 0.732421875
                                attr 2: scale_available value: 0.732421875 1.464843750
                        temp:  (input)
                        3 channel-specific attributes found:
                                attr 0: offset value: -628
                                attr 1: raw value: 680
                                attr 2: scale value: 452.147700000

IIO sysfs interface

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# ls -al
total 0
drwxr-xr-x 3 root root    0 Jan  1  1970 .
drwxr-xr-x 5 root root    0 Jan  1  1970 ..
-rw-rw-rw- 1 root root 4096 Jan  1  1970 dev
-rw-rw-rw- 1 root root 4096 Jan  1  1970 in_temp_offset
-rw-rw-rw- 1 root root 4096 Jan  1  1970 in_temp_raw
-rw-rw-rw- 1 root root 4096 Jan  1  1970 in_temp_scale
-rw-rw-rw- 1 root root 4096 Jan  1  1970 in_voltage1_raw
-rw-rw-rw- 1 root root 4096 Jan  1  1970 in_voltage2_raw
-rw-rw-rw- 1 root root 4096 Jan  1  1970 in_voltage3_raw
-rw-rw-rw- 1 root root 4096 Jan  1  1970 in_voltage_scale
-rw-rw-rw- 1 root root 4096 Jan  1  1970 in_voltage_scale_available
-rw-rw-rw- 1 root root 4096 Jan  1  1970 name
lrwxrwxrwx 1 root root    0 Jan  1  1970 of_node -> ../../../../../../../firmware/devicetree/base/amba/i2c@e0004000/ad5593r@10
-rw-rw-rw- 1 root root 4096 Jan  1  1970 out_voltage0_raw
-rw-rw-rw- 1 root root 4096 Jan  1  1970 out_voltage2_raw
-rw-rw-rw- 1 root root 4096 Jan  1  1970 out_voltage3_raw
-rw-rw-rw- 1 root root 4096 Jan  1  1970 out_voltage_scale
-rw-rw-rw- 1 root root 4096 Jan  1  1970 out_voltage_scale_available
drwxrwxrwx 2 root root    0 Jan  1  1970 power
lrwxrwxrwx 1 root root    0 Jan  1  1970 subsystem -> ../../../../../../../bus/iio
-rw-rw-rw- 1 root root 4096 Jan  1  1970 uevent
root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# 
root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# grep "" *
dev:252:2
in_temp_offset:-753
in_temp_raw:810
in_temp_scale:376.789750000
in_voltage1_raw:0
in_voltage2_raw:0
in_voltage3_raw:0
in_voltage_scale:0.610351562
in_voltage_scale_available:0.610351562 1.220703124
name:ad5592r
out_voltage0_raw:0
out_voltage2_raw:0
out_voltage3_raw:0
out_voltage_scale:0.610351562
out_voltage_scale_available:0.610351562 1.220703124
uevent:MINOR=2
uevent:DEVNAME=iio:device2
uevent:DEVTYPE=iio_device
uevent:OF_NAME=ad5593r
uevent:OF_FULLNAME=/amba/i2c@e0004000/ad5593r@10
uevent:OF_COMPATIBLE_0=adi,ad5593r
uevent:OF_COMPATIBLE_N=1

Show device name

This specifies any shell prompt running on the target

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# cat name
ad5593r

Scales

The output range of the DAC is 0 V to VREF or 0 V to 2 × VREF. out_voltage_scale is used to select the high or low range. Without external reference the driver selects the internal 2500mV VREF reference. So the scale computes as 2500mV/2^12 = 0.610351562 or 5000mV/2^12 = 1.220703124.

The input range of the ADC is 0 V to VREF or 0 V to 2 × VREF. in_voltage_scale is used to select the high or low range. Without external reference the driver selects the internal 2500mV VREF reference. So the scale computes as 2500mV/2^12 = 0.610351562 or 5000mV/2^12 = 1.220703124.

Show current scale

Description:
scale to be applied to out_voltageY_raw/in_voltageY_raw in order to obtain the measured voltage in millivolts.

This specifies any shell prompt running on the target

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# cat out_voltage_scale
0.610351562

Show available scales

Description:
scale to be applied to out_voltageY_raw/in_voltageY_raw in order to obtain the measured voltage in millivolts.

This specifies any shell prompt running on the target

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# cat in_voltage_scale_available
0.610351562 1.220703124

Change scales

Description:
scale to be applied to out_voltageY_raw/in_voltageY_raw in order to obtain the measured voltage in millivolts.

This specifies any shell prompt running on the target

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# echo 1.220703124 > in_voltage_scale
root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# cat in_voltage_scale
1.220703124

Get channel Y input voltage

Description: Raw unscaled voltage measurement on channel Y

This specifies any shell prompt running on the target

This specifies any shell prompt running on the target

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# cat in_voltage3_raw
1491

U = in_voltage3_raw * in_voltage_scale = 1491 * 0.610351562 = 910 mV

Set channel Y output voltage

Description:
Raw (unscaled, no bias etc.) output voltage for channel Y.

This specifies any shell prompt running on the target

root@linaro-ubuntu-desktop:/sys/bus/iio/devices/iio:device2# echo 1638 > out_voltage0_raw

U = out_voltage0_raw * out_voltage_scale = 1638 * 0.610351562 = 999.76 mV

Example obtaining the temperature in °C

T = ( in_temp_raw + in_temp_offset ) * in_temp_scale

T = ( 810 - 753 ) * 376.78975 = 21477 mdeg C = 21.5 °C

For more information see also here: IIO Kernel Documentation

GPIO Testing

The GPIO sysfs interface allows users to manipulate any GPIO from userspace. Userspace utilizes a sysfs control interface to dynamically request and release individual GPIOs. Once a GPIO has been requested, writing to the newly created path allows you to control the direction and the data while reading from it returns the GPIO data (which usually corresponds to a 0 or 1 which represents the signal level).

For more information see also here: GPIO Kernel Documentation

root@linaro-ubuntu-desktop:~# cd /sys/class/gpio/
root@linaro-ubuntu-desktop:/sys/class/gpio# ls
export  gpiochip890  gpiochip898  gpiochip906  unexport

root@linaro-ubuntu-desktop:/sys/class/gpio# cd gpiochip890

root@linaro-ubuntu-desktop:/sys/class/gpio/gpiochip890# ls -al
total 0
drwxr-xr-x 3 root root    0 Jan  1  1970 .
drwxr-xr-x 3 root root    0 Jan  1  1970 ..
-r--r--r-- 1 root root 4096 Feb 23 08:06 base
lrwxrwxrwx 1 root root    0 Feb 23 08:06 device -> ../../../0-0010
-r--r--r-- 1 root root 4096 Feb 23 08:06 label
-r--r--r-- 1 root root 4096 Feb 23 08:06 ngpio
drwxr-xr-x 2 root root    0 Feb 23 08:06 power
lrwxrwxrwx 1 root root    0 Jan  1  1970 subsystem -> ../../../../../../../../class/gpio
-rw-r--r-- 1 root root 4096 Jan  1  1970 uevent

root@linaro-ubuntu-desktop:/sys/class/gpio/gpiochip890# grep "" *
base:890
label:0-0010
ngpio:8


root@linaro-ubuntu-desktop:/sys/class/gpio/gpiochip890# cd ..
root@linaro-ubuntu-desktop:/sys/class/gpio# echo 897 > export 
root@linaro-ubuntu-desktop:/sys/class/gpio# cd gpio897/
root@linaro-ubuntu-desktop:/sys/class/gpio/gpio897# ls -al
total 0
drwxr-xr-x 3 root root    0 Feb 23 08:06 .
drwxr-xr-x 4 root root    0 Feb 23 08:06 ..
-rw-r--r-- 1 root root 4096 Feb 23 08:06 active_low
lrwxrwxrwx 1 root root    0 Feb 23 08:06 device -> ../../../0-0010
-rw-r--r-- 1 root root 4096 Feb 23 08:06 direction
drwxr-xr-x 2 root root    0 Feb 23 08:06 power
lrwxrwxrwx 1 root root    0 Feb 23 08:06 subsystem -> ../../../../../../../../class/gpio
-rw-r--r-- 1 root root 4096 Feb 23 08:06 uevent
-rw-r--r-- 1 root root 4096 Feb 23 08:06 value

root@linaro-ubuntu-desktop:/sys/class/gpio/gpio897# cat direction 
in

root@linaro-ubuntu-desktop:/sys/class/gpio/gpio897# cat value 
0

root@linaro-ubuntu-desktop:/sys/class/gpio/gpio897# echo low > direction 

root@linaro-ubuntu-desktop:/sys/class/gpio/gpio897# cat direction 
out

root@linaro-ubuntu-desktop:/sys/class/gpio/gpio897# cat value 
0

root@linaro-ubuntu-desktop:/sys/class/gpio/gpio897# echo high > direction                                                                                                                                    

root@linaro-ubuntu-desktop:/sys/class/gpio/gpio897# cat value 
1
resources/tools-software/linux-drivers/iio-dac/ad5593r.txt · Last modified: 19 Jan 2018 10:12 by Alexandru Ardelean