NOTE:
This driver is RETIRED, DEPRECATED and not used anymore in any of the recent projects!
Please see here instead: ADI JESD204B/C AXI_ADXCVR Highspeed Transceivers Linux Driver
This driver supports the
The AXI JESD204 GT HDL driver is the driver for the Gigabit Tranceiver (GTX, GTH, etc.) HDL interface core which is used on various FPGA designs. The driver is implemented as an Open Firmware Device Tree (DT) platform driver. It's register map can be found here: Base register map (common to all cores)
This driver is used by the JESD Eye Scan - See here JESD204 Eye Scan
Source | Mainlined? |
---|---|
drivers/iio/jesd204/axi_jesd204b_gt.c | WIP |
Function | File |
---|---|
driver | drivers/iio/jesd204/axi_jesd204b_gt.c |
include | drivers/iio/jesd204/axi_jesd204b_gt.h |
The AXI JESD204B driver is a platform driver and can currently only be instantiated via device tree. Depending on which HDL Version (PCORE_VERSION) the HDL supports two links, one receive and one transmit, depending on [rx|tx]-[sys|out]-clk-select is given both or not.
Starting with PCORE_VERSION > 7.0.0, the HDL and driver supports multiple links. And the setup is done per lane basis. The device tree entry then features multiple per link child nodes.
Required devicetree properties (legacy (flat) mode & PCORE_VERSION < 7.0.0):
Required devicetree properties (PCORE_VERSION > 7.0.0):
Example:
axi_daq2_gt: axi-jesd-gt-rx-tx@44a60000 { #address-cells = <1>; #size-cells = <0>; #clock-cells = <1>; compatible = "xlnx,axi-jesd-gt-1.0"; reg = < 0x44a60000 0x10000 >; axi_daq2_gt_rx0:link@0 { #clock-cells = <0>; clocks = <&clk0_ad9523 1>, <&clk0_ad9523 6>; clock-names = "conv", "sysref"; clock-output-names = "adc_gt_clk"; reg = <0>; adi,lanes = <4>; adi,first-lane = <0>; adi,sys-clk-select = <3>; adi,out-clk-select = <4>; adi,use-lpm-enable; }; axi_daq2_gt_tx0:link@1 { #clock-cells = <0>; clocks = <&clk0_ad9523 7>, <&clk0_ad9523 13>; clock-names = "conv", "sysref"; clock-output-names = "dac_gt_clk"; reg = <0>; adi,lanes = <4>; adi,first-lane = <0>; adi,link-is-transmit-enable; adi,sys-clk-select = <3>; adi,out-clk-select = <4>; adi,use-lpm-enable; }; } ;
Example (legacy mode):
axi_daq2_gt: axi-jesd-gt-rx-tx@44a60000 { #clock-cells = <1>; compatible = "xlnx,axi-jesd-gt-1.0"; reg = < 0x44a60000 0x10000 >; clocks = <&clk0_ad9523 1>, <&clk0_ad9523 6>, <&clk0_ad9523 7>, <&clk0_ad9523 13>; clock-names = "adc_clk", "adc_sysref", "dac_sysref", "dac_clk"; clock-output-names = "adc_gt_clk", "dac_gt_clk"; adi,rx-sys-clk-select = <3>; adi,rx-out-clk-select = <4>; adi,tx-sys-clk-select = <3>; adi,tx-out-clk-select = <4>; adi,lanes = <0x4>; adi,use-lpm-enable; } ;
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Device Drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support *** Analog to digital converters *** [--snip--] <*> Generic AXI JESD204B configuration driver [--snip--]
# cd 44a60000.axi-jesd-gt/ # ls -al total 0 drwxr-xr-x 2 root root 0 Jan 1 00:21 . drwxr-xr-x 25 root root 0 Jan 1 00:00 .. lrwxrwxrwx 1 root root 0 Jan 1 00:24 driver -> ../../../bus/platform/drivers/cf_axi_jesd204b_gt -rw-r--r-- 1 root root 4096 Jan 1 00:24 driver_override --w------- 1 root root 4096 Jan 1 00:24 enable -r-------- 1 root root 132600 Jan 1 00:24 eye_data -r-------- 1 root root 4096 Jan 1 00:24 info -r--r--r-- 1 root root 4096 Jan 1 00:24 modalias --w------- 1 root root 4096 Jan 1 00:24 prescale -rw------- 1 root root 4096 Jan 1 00:24 reg_access lrwxrwxrwx 1 root root 0 Jan 1 00:24 subsystem -> ../../../bus/platform -rw-r--r-- 1 root root 4096 Jan 1 00:24 uevent # cat info x65,y255 CDRDW: 40