Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:tools-software:linux-drivers:iio-adc:axi-adc-hdl [18 Mar 2021 17:54] – [Supported Boards] Michael Hennerichresources:tools-software:linux-drivers:iio-adc:axi-adc-hdl [13 Jun 2022 13:11] (current) – [Driver testing] Michael Hennerich
Line 321: Line 321:
 </xterm></WRAP> </xterm></WRAP>
  
 +=== External Synchronization ===
  
-in_voltage0_test_mode:off+The [[resources:fpga:peripherals:jesd204:jesd204_tpl_adc|ADC TPL HDL]] core supports the [[resources:fpga:peripherals:jesd204:jesd204_tpl_adc#External_synchronization|EXT_SYNC]] feature, allowing to synchronize multiple channels within a ADC or across multiple instances. 
 +This feature can also synchronize between the [[resources:fpga:peripherals:jesd204:jesd204_tpl_adc|ADC TPL HDL]] and [[resources:fpga:peripherals:jesd204:jesd204_tpl_dac|DAC TPL HDL]] core.  
 + 
 +There are two device attributes which allows controlling this feature: 
 +''sync_start_enable'' and ''sync_start_enable_available'' reading the 
 +later returns the available modes which depend on HDL core synthesis 
 +parameters. The options are explained below. Reading 'sync_start_enable' 
 +returns either 'arm' while waiting for the external synchronization 
 +signal or 'disarm' otherwise. 
 + 
 +  * ''arm'': Setting this key will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a ADC, and across multiple instances. This key has an effect only the EXT_SYNC synthesis parameter is set.  
 + 
 +  * ''disarm'': Setting this key will disarm the trigger mechanism sensitive to an external sync signal. This key has an effect only the EXT_SYNC synthesis parameter is set. 
 + 
 +  * ''trigger_manual'': Setting this key will issue an external sync event if it is hooked up inside the fabric. This key has an effect only the EXT_SYNC synthesis parameter is set. 
 +         
 +== Example: == 
 + 
 +<WRAP box bggreen><wrap info>This specifies any shell prompt running on the target</wrap> 
 +<xterm> 
 +root@analog:/sys/bus/iio/devices/iio:device3# **cat sync_start_enable_available**                                                                                                                        
 +**arm disarm trigger_manual** 
 +root@analog:/sys/bus/iio/devices/iio:device3# **cat sync_start_enable** 
 +**disarm** 
 +root@analog:/sys/bus/iio/devices/iio:device3# **echo arm > sync_start_enable**                                                                                                                                  
 +root@analog:/sys/bus/iio/devices/iio:device3# **cat sync_start_enable** 
 +**arm** 
 +root@analog:/sys/bus/iio/devices/iio:device3# **echo trigger_manual > sync_start_enable**                                                                                                                       
 +root@analog:/sys/bus/iio/devices/iio:device3# **cat sync_start_enable** 
 +**disarm** 
 +</xterm></WRAP>
 ===== Buffer management ===== ===== Buffer management =====
  
resources/tools-software/linux-drivers/iio-adc/axi-adc-hdl.txt · Last modified: 13 Jun 2022 13:11 by Michael Hennerich