Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
Next revision
Previous revision
resources:tools-software:linux-drivers:iio-adc:ad9208 [21 Jan 2022 16:37]
Michael Hennerich [Example devicetree SPI device initialization]
resources:tools-software:linux-drivers:iio-adc:ad9208 [21 Jan 2022 17:15]
Michael Hennerich [Hardware configuration]
Line 160: Line 160:
  
  /* JESD204 parameters */  /* JESD204 parameters */
- adi,converters-per-device ​= <2>; /* JESD204 (M) */ + adi,octets-per-frame = <1>; 
- adi,lanes-per-device ​= <4>; /* JESD204 (L) */ + adi,frames-per-multiframe ​= <32>; 
- adi,octets-per-frame ​= <1>; /* JESD204 (F) */ + adi,converter-resolution ​= <16>; 
- adi,frames-per-multiframe ​= <32>; /* JESD204 (K) */ + adi,bits-per-sample ​= <16>; 
- adi,converter-resolution ​= <14>; /* JESD204 (N) */ + adi,converters-per-device ​= <2>; 
- adi,​bits-per-sample = <16>; /* JESD204 (N') */ + adi,control-bits-per-sample = <0>; 
- adi,control-bits-per-sample ​= <2>; /* JESD204 (CS) */ + adi,lanes-per-device ​= <8>; 
- adi,​subclass = <1>; /* JESD204 (SUBCLASSV) */+ adi,​subclass = <1>;
  
  /* DDC setup */  /* DDC setup */
Line 201: Line 201:
  spi-max-frequency = <​1000000>;​  spi-max-frequency = <​1000000>;​
  
- clocks = <&​axi_ad9680_jesd>, ​<&​clk0_ad9523 13>, <&​clk0_ad9523 5>; + clocks = <&​clk0_ad9523 13>; 
- clock-names = "​jesd_adc_clk", ​"​adc_clk", "​adc_sysref";+ clock-names = "​adc_clk";​
  
  /* jesd204-fsm support */  /* jesd204-fsm support */
Line 224: Line 224:
  /* JESD204 parameters */  /* JESD204 parameters */
  
- adi,octets-per-frame = <1>; + adi,converters-per-device ​= <2>; /* JESD204 (M) */ 
- adi,frames-per-multiframe ​= <32>; + adi,lanes-per-device ​= <4>; /* JESD204 (L) */ 
- adi,converter-resolution ​= <14>; + adi,octets-per-frame ​= <1>; /* JESD204 (F) */ 
- adi,bits-per-sample ​= <16>; + adi,frames-per-multiframe ​= <32>; /* JESD204 (K) */ 
- adi,converters-per-device ​= <2>; + adi,converter-resolution ​= <14>; /* JESD204 (N) */ 
- adi,control-bits-per-sample = <2>; + adi,​bits-per-sample = <16>; /* JESD204 (N') */ 
- adi,lanes-per-device ​= <4>; + adi,control-bits-per-sample ​= <2>; /* JESD204 (CS) */ 
- adi,​subclass = <1>;+ adi,​subclass = <1>; /* JESD204 (SUBCLASSV) */
  
  /* DDC setup */  /* DDC setup */
Line 295: Line 295:
 </​xterm>​ </​xterm>​
  
 +
 +**AD9680 using:** [[resources:​tools-software:​linux-drivers:​jesd204:​jesd204-fsm-framework|JESD204 (FSM) Interface Linux Kernel Framework]]
 +
 +<wrap info>​This specifies the root console running on the target</​wrap>​
 +<​xterm>​
 +axi_adxcvr 44a50000.axi-adxcvr-rx:​ AXI-ADXCVR-RX (17.05.a) using QPLL on GTX2 at 0x44A50000. Number of lanes: 4.
 +axi-jesd204-rx 44aa0000.axi-jesd204-rx:​ AXI-JESD204-RX (1.07.a) at 0x44AA0000. Encoder 8b10b, width 4/4, lanes 4, jesd204-fsm.
 +ad9208 spi0.2: ad9680 PLL LOCKED
 +ad9208 spi0.2: ad9680 Rev. 2 Grade 10 (API 1.0.1) probed
 +cf_axi_adc 44a10000.axi-ad9680-hpc:​ ADI AIM (10.01.b) at 0x44A10000 mapped to 0x7d3c02c1, probed ADC AD9680 as MASTER
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition initialized -> probed
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition probed -> idle
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition idle -> device_init
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition device_init -> link_init
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition link_init -> link_supported
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition link_supported -> link_pre_setup
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition link_pre_setup -> clk_sync_stage1
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition clk_sync_stage1 -> clk_sync_stage2
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition clk_sync_stage2 -> clk_sync_stage3
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition clk_sync_stage3 -> link_setup
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition link_setup -> opt_setup_stage1
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition opt_setup_stage1 -> opt_setup_stage2
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition opt_setup_stage2 -> opt_setup_stage3
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition opt_setup_stage3 -> opt_setup_stage4
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition opt_setup_stage4 -> opt_setup_stage5
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition opt_setup_stage5 -> clocks_enable
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition clocks_enable -> link_enable
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition link_enable -> link_running
 +jesd204: /​axi/​spi@e0006000/​ad9680@2,​jesd204:​1,​parent=spi0.2:​ JESD204[0] transition link_running -> opt_post_running_stage
 +</​xterm>​
 ====== Driver testing ====== ====== Driver testing ======
  
resources/tools-software/linux-drivers/iio-adc/ad9208.txt · Last modified: 21 Jan 2022 17:15 by Michael Hennerich