This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linux-drivers:iio-adc:ad7606 [18 Apr 2019 14:55] – update the name of ad7606b eval board Stefan Popa | resources:tools-software:linux-drivers:iio-adc:ad7606 [30 Sep 2019 09:03] (current) – Add 7616 to the list Beniamin Bia | ||
---|---|---|---|
Line 8: | Line 8: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
===== Reference Circuits ===== | ===== Reference Circuits ===== | ||
Line 20: | Line 21: | ||
* [[adi> | * [[adi> | ||
* [[adi> | * [[adi> | ||
+ | * [[adi> | ||
===== Description ===== | ===== Description ===== | ||
Line 39: | Line 41: | ||
| driver | | driver | ||
| include | [[git.linux.org> | | include | [[git.linux.org> | ||
+ | | documentation| [[git.linux.org> | ||
====== Example platform device initialization ====== | ====== Example platform device initialization ====== | ||
Line 52: | Line 55: | ||
| AD7606-6 | ad7606-6 | | | AD7606-6 | ad7606-6 | | ||
| AD7606-4 | ad7606-4 | | | AD7606-4 | ad7606-4 | | ||
+ | | AD7606B | ad7606b | | ||
+ | | AD7616 | ad7616 | | ||
<code c> | <code c> | ||
Line 180: | Line 185: | ||
* " | * " | ||
* " | * " | ||
+ | * " | ||
- reg: SPI chip select number for the device | - reg: SPI chip select number for the device | ||
- spi-max-frequency: | - spi-max-frequency: |