Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:linux-drivers:iio-adc:ad6676 [11 Feb 2016 21:07] – [Status] Lars-Peter Clausenresources:tools-software:linux-drivers:iio-adc:ad6676 [19 Jan 2021 08:28] (current) – [Driver testing / API] Michael Hennerich
Line 27: Line 27:
  
 ^ Source ^ Mainlined? ^ ^ Source ^ Mainlined? ^
-| [[linux.github>xcomm_zynq?drivers/iio/adc/ad6676.c|git]] | [[linux.github>xcomm_zynq?drivers/iio/adc/ad6676.c|No]] |+| [[linux.github>master?drivers/iio/adc/ad6676.c|git]] | [[linux.github>master?drivers/iio/adc/ad6676.c|No]] |
  
 ===== Files ===== ===== Files =====
  
 ^ Function ^ File ^ ^ Function ^ File ^
-| driver  | [[linux.github>xcomm_zynq?drivers/iio/adc/ad6676.c | drivers/iio/adc/ad6676.c]] | +| driver  | [[linux.github>master?drivers/iio/adc/ad6676.c | drivers/iio/adc/ad6676.c]] | 
-| include | [[linux.github>xcomm_zynq?drivers/iio/adc/ad6676.h | drivers/iio/adc/ad6676.h]] |+| include | [[linux.github>master?drivers/iio/adc/ad6676.h | drivers/iio/adc/ad6676.h]] |
  
 ==== Related Device Drivers ==== ==== Related Device Drivers ====
  
 ^ Function ^ File ^ ^ Function ^ File ^
-| driver  | [[linux.github>xcomm_zynq?drivers/iio/adc/cf_axi_adc_core.c | drivers/iio/adc/cf_axi_adc_core.c]] | +| driver  | [[linux.github>master?drivers/iio/adc/cf_axi_adc_core.c | drivers/iio/adc/cf_axi_adc_core.c]] | 
-| driver  | [[linux.github>xcomm_zynq?drivers/iio/adc/cf_axi_adc_ring_stream.c | drivers/iio/adc/cf_axi_adc_ring_stream.c]] | +| driver  | [[linux.github>master?drivers/iio/adc/cf_axi_adc_ring_stream.c | drivers/iio/adc/cf_axi_adc_ring_stream.c]] | 
-| include | [[linux.github>xcomm_zynq?drivers/iio/adc/cf_axi_adc.h | drivers/iio/adc/cf_axi_adc.h]] |+| include | [[linux.github>master?drivers/iio/adc/cf_axi_adc.h | drivers/iio/adc/cf_axi_adc.h]] |
  
  
Line 52: Line 52:
  
 ^ Function ^ File ^ ^ Function ^ File ^
-FMCOMMS2/Device Tree  | [[linux.github>xcomm_zynq?arch/arm/boot/dts/zynq-zc706-adv7511-ad6676-fmc.dts+AD6676-EBZ Device Tree  | [[linux.github>master?arch/arm/boot/dts/zynq-zc706-adv7511-ad6676-fmc.dts
 | zynq-zc706-adv7511-ad6676-fmc.dts]] | | zynq-zc706-adv7511-ad6676-fmc.dts]] |
  
Line 69: Line 69:
 | adi,bandwidth-margin-high-mhz         | Initial bandwidth margin high in Hz | | adi,bandwidth-margin-high-mhz         | Initial bandwidth margin high in Hz |
 | adi,bandwidth-margin-if-mhz           | Initial bandwidth margin IF in Hz | | adi,bandwidth-margin-if-mhz           | Initial bandwidth margin IF in Hz |
-| adi,external-inductance-l-nh          | The inductance of the external inductors in nH|+| adi,external-inductance-l-nh          | The inductance of the external inductors in nH |
 | adi,idac1-fullscale-adjust            | Initial IDAC_FS [64..16] | | adi,idac1-fullscale-adjust            | Initial IDAC_FS [64..16] |
 | adi,shuffler-control                  | Initial shuffler control setting | | adi,shuffler-control                  | Initial shuffler control setting |
 | adi,shuffler-thresh                   | Initial shuffler threshold| | adi,shuffler-thresh                   | Initial shuffler threshold|
-| adi,jesd-scrambling-enable            | Enables JESD scrambling |+| adi,jesd-scrambling-enable            | Enables JESD204B link scrambling |
 | adi,jesd-use-lvds-syncb-enable        | Use LVDS SYNCB | | adi,jesd-use-lvds-syncb-enable        | Use LVDS SYNCB |
 | adi,jesd-powerdown-sysref-enable      | Powerdown SYSREF | | adi,jesd-powerdown-sysref-enable      | Powerdown SYSREF |
-| adi,jesd-l-lanes                      | Number of JESD lanes|+| adi,jesd-l-lanes                      | Number of JESD204B lanes |
 | adi,jesd-f-frames-per-multiframe      | Number of frames per multiframe | | adi,jesd-f-frames-per-multiframe      | Number of frames per multiframe |
 | adi,spi-3wire-enable                  | Enables SPI 3-WIRE mode | | adi,spi-3wire-enable                  | Enables SPI 3-WIRE mode |
Line 122: Line 122:
 An example program which uses the interface can be found here: An example program which uses the interface can be found here:
   * [[resources:tools-software:linux-software:iio_oscilloscope|IIO Oscilloscope]]   * [[resources:tools-software:linux-software:iio_oscilloscope|IIO Oscilloscope]]
-  * [[resources:tools-software:linux-software:ad6676ebz_plugin|AD6676-EBZ GUI Plugin Description]] 
  
 {{ :resources:tools-software:linux-drivers:iio-adc:ad6676-osc-screenshot.png?600 |}} {{ :resources:tools-software:linux-drivers:iio-adc:ad6676-osc-screenshot.png?600 |}}
Line 193: Line 192:
 <WRAP top tip round box 60%>**TIP:** <WRAP top tip round box 60%>**TIP:**
 If writing this attribute returns "Invalid argument" (-EINVAL) this means that the underlying If writing this attribute returns "Invalid argument" (-EINVAL) this means that the underlying
-HDL or Hardware'JESD Core and Gigabit Transceiver (GT) doesn't support changing the JESD Lane Rate.+HDL or Hardware'JESD204B Core and Gigabit Transceiver (GT) doesn't support changing the JESD204B Lane Rate.
  
 </WRAP>\\ </WRAP>\\
Line 203: Line 202:
 The complex (I/Q) data rate at the JESD204B outputs is FADC / DF. The complex (I/Q) data rate at the JESD204B outputs is FADC / DF.
  
-In case the underlying HDL or Hardware'JESD Core and Gigabit Transceiver (GT) support arbitrary JESD Lane Rates.+In case the underlying HDL or Hardware'JESD204B Core and Gigabit Transceiver (GT) support arbitrary JESD204B Lane Rates.
 This attribute can be writable. And it will select the appropriate AD6676 supported DFs. This attribute can be writable. And it will select the appropriate AD6676 supported DFs.
  
Line 388: Line 387:
 </xterm></WRAP> </xterm></WRAP>
  
-===== JESD Interface Testing =====+===== JESD204B Interface Testing =====
  
 Below Eyes were captured on a Xilinx ZC706 after > 4 hours of operation: Below Eyes were captured on a Xilinx ZC706 after > 4 hours of operation:
  
-[[resources:tools-software:linux-software:jesd_eye_scan|JESD204 Eye Scan]] +[[resources:tools-software:linux-software:jesd_eye_scan|JESD204B Eye Scan]] 
  
 {{:resources:tools-software:linux-drivers:iio-adc:ad6676_lane0_9.54e-08bert.png?300 | LANE0}} {{:resources:tools-software:linux-drivers:iio-adc:ad6676_lane0_9.54e-08bert.png?300 | LANE0}}
resources/tools-software/linux-drivers/iio-adc/ad6676.txt · Last modified: 19 Jan 2021 08:28 by Michael Hennerich