Wiki

This version (07 Jan 2020 13:50) was approved by nsa.The Previously approved version (20 Aug 2019 13:44) is available.Diff

LTC2947 High Precision Power and Energy Monitor

Supported Devices

Evaluation Boards

Description

This is a Hardware Monitor subsystem driver. There are two driver's (sharing the same core implementation) for the LTC2947 since the device supports both SPI and I2C interfaces. The underlying bus is abstracted in the core implementation by using regmap. The Hwmon subsystem provides a unified framework for drivers doing hardware monitoring. It exposes a set of sysfs file that should follow the sysfs-interface.

Source Code

Status

Files

Example I2C & SPI device initialization

The LTC2947 supports both I2C and SPI interfaces, so one of the drivers can be used depending on which kind of device is instantiated. Currently, the devices can only be instantiated via device tree.

Required devicetree properties:

  • compatible: Must be always one of these:
    • adi,ltc2947
  • reg: Must be either the I2C device address or the SPI device chip select number.

Example SPI:

&spi0 {
        #address-cells = <1>;
        #size-cells = <0>;
        status = "okay";
        ltc2947_spi: ltc2947@0 {
                compatible = "adi,ltc2947";
                reg = <0>;
                spi-max-frequency = <1000000>;
        };
};

Example I2C:

&i2c0 {
        #address-cells = <1>;
        #size-cells = <0>;
        status = "okay";
        ltc2947_i2c: ltc2947@5c {
                compatible = "adi,ltc2947";
                reg = <0x5c>;
        };
};

For more supported devicetree properties take a look to dt-bindings.

Enabling Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”).

The LTC2947 SPI driver depends CONFIG_SPI and the LTC2947 I2C driver depends on CONFIG_I2C.

Adding Linux driver support

Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)

Linux Kernel Configuration
	Device Drivers  --->
        <*>     Hardware Monitoring support --->
            --- Hardware Monitoring support
        [--snip--]
            <*> Analog Devices LTC2947 High Precision Power and Energy Monitor over I2C
            <*> Analog Devices LTC2947 High Precision Power and Energy Monitor over SPI
        [--snip--]

Hardware configuration

Driver testing

HWMON device files

Each and every HWMON device has a device folder under /sys/class/hwmon/hwmonX, where X is the hwmon device index. Under every of these directory folders there are a set of files, depending on what kind of hardware monitoring is supported (temperature, voltage). In order to determine which hwmon device corresponds to which hardware chip, the user can read the name file under /sys/class/hwmon/hwmonX/name.

This specifies any shell prompt running on the target

root:/> cd /sys/class/hwmon/
root:/sys/class/hwmon> ls
hwmon0  hwmon1

root:/sys/class/hwmon> cd hwmon1

root:/sys/class/hwmon/hwmon1> ls -l
total 0
-r--r--r-- 1 root root 4096 Nov 16 09:25 curr1_fault
-r--r--r-- 1 root root 4096 Nov 16 09:25 curr1_highest
-r--r--r-- 1 root root 4096 Nov 16 09:25 curr1_input
-r--r--r-- 1 root root 4096 Nov 16 09:25 curr1_label
-r--r--r-- 1 root root 4096 Nov 16 09:25 curr1_lowest
-rw-r--r-- 1 root root 4096 Nov 16 09:25 curr1_max
-r--r--r-- 1 root root 4096 Nov 16 09:25 curr1_max_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:25 curr1_min
-r--r--r-- 1 root root 4096 Nov 16 09:25 curr1_min_alarm
--w------- 1 root root 4096 Nov 16 09:25 curr1_reset_history
lrwxrwxrwx 1 root root    0 Nov 16 09:25 device -> ../../../spi0.0
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy1_fault
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy1_input
-rw-r--r-- 1 root root 4096 Nov 16 09:25 energy1_max
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy1_max_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:25 energy1_min
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy1_min_alarm
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy1_overflow_alarm
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy2_fault
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy2_input
-rw-r--r-- 1 root root 4096 Nov 16 09:25 energy2_max
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy2_max_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:25 energy2_min
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy2_min_alarm
-r--r--r-- 1 root root 4096 Nov 16 09:25 energy2_overflow_alarm
-r--r--r-- 1 root root 4096 Nov 16 09:25 in0_fault
-r--r--r-- 1 root root 4096 Nov 16 09:25 in0_highest
-r--r--r-- 1 root root 4096 Nov 16 09:25 in0_input
-r--r--r-- 1 root root 4096 Nov 16 09:25 in0_label
-r--r--r-- 1 root root 4096 Nov 16 09:25 in0_lowest
-rw-r--r-- 1 root root 4096 Nov 16 09:25 in0_max
-r--r--r-- 1 root root 4096 Nov 16 09:25 in0_max_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:25 in0_min
-r--r--r-- 1 root root 4096 Nov 16 09:25 in0_min_alarm
--w------- 1 root root 4096 Nov 16 09:25 in0_reset_history
-r--r--r-- 1 root root 4096 Nov 16 09:25 in1_fault
-r--r--r-- 1 root root 4096 Nov 16 09:25 in1_highest
-r--r--r-- 1 root root 4096 Nov 16 09:25 in1_input
-r--r--r-- 1 root root 4096 Nov 16 09:25 in1_label
-r--r--r-- 1 root root 4096 Nov 16 09:25 in1_lowest
-rw-r--r-- 1 root root 4096 Nov 16 09:25 in1_max
-r--r--r-- 1 root root 4096 Nov 16 09:25 in1_max_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:25 in1_min
-r--r--r-- 1 root root 4096 Nov 16 09:25 in1_min_alarm
--w------- 1 root root 4096 Nov 16 09:25 in1_reset_history
-r--r--r-- 1 root root 4096 Nov 16 09:21 name
lrwxrwxrwx 1 root root    0 Nov 16 09:25 of_node -> ../../../../../../../../../firmware/devicetree/base/soc/spi@7e204000/ltc2947@0
drwxr-xr-x 2 root root    0 Nov 16 09:25 power
-r--r--r-- 1 root root 4096 Nov 16 09:25 power1_fault
-r--r--r-- 1 root root 4096 Nov 16 09:25 power1_input
-r--r--r-- 1 root root 4096 Nov 16 09:25 power1_input_highest
-r--r--r-- 1 root root 4096 Nov 16 09:25 power1_input_lowest
-r--r--r-- 1 root root 4096 Nov 16 09:25 power1_label
-rw-r--r-- 1 root root 4096 Nov 16 09:25 power1_max
-r--r--r-- 1 root root 4096 Nov 16 09:25 power1_max_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:25 power1_min
-r--r--r-- 1 root root 4096 Nov 16 09:25 power1_min_alarm
--w------- 1 root root 4096 Nov 16 09:25 power1_reset_history
lrwxrwxrwx 1 root root    0 Nov 16 09:25 subsystem -> ../../../../../../../../../class/hwmon
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp1_fault
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp1_highest
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp1_input
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp1_label
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp1_lowest
-rw-r--r-- 1 root root 4096 Nov 16 09:25 temp1_max
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp1_max_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:25 temp1_min
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp1_min_alarm
--w------- 1 root root 4096 Nov 16 09:25 temp1_reset_history
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp2_label
-rw-r--r-- 1 root root 4096 Nov 16 09:25 temp2_max
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp2_max_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:25 temp2_min
-r--r--r-- 1 root root 4096 Nov 16 09:25 temp2_min_alarm
-rw-r--r-- 1 root root 4096 Nov 16 09:17 uevent
root:/sys/class/hwmon/hwmon1>

For each type of monitored value (current, power), the file will look like ${type}_${monitored_value}_${channel}, where ${monitored_value} can be the current value, the high threshold, etc… The channel is the index when, for example, a device can monitor more than one voltage. For more information on the files format, take a look to sysfs-interface.

Show device name

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat name
ltc2947

Show current values

The device supports readings of current, voltage, power, temperature and energy. To get, for example, the value of the monitored voltage:

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in0_input
4910

Show highest read value

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in0_highest
5026

Show lowest read value

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in0_lowest
4754

Show high threshold

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in0_max
5500

Show low threshold

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in0_min
4500

Show high threshold alarm

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in0_max_alarm
0

Show low threshold alarm

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in0_min_alarm
0

Show fault

When the ${type}_${channel}_fault files are present, the user can read these files to look for faulty cases. If reading this file returns 1, then the readings for that channel are invalid and should be discarded…

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in0_fault
0

Show label

Some channels, support a label attribute which specifies the name of the channel being monitored.

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat in1_label
DVCC

Show Overflow alarm

These properties are custom and not part of the sysfs-hwmon interface. However, the device set's an alarm when register overflow is near for accumulated values (in this case, energy).

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> cat energy1_overflow_alarm
0

Set High threshold

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> echo 5500 > in0_max

Set Low threshold

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> echo 4500 > in0_min

Reset History

This specifies any shell prompt running on the target

root:/sys/class/hwmon/hwmon1> echo 1 > in0_reset_history

More Information

HWMON pointers

31 Jul 2012 17:53 · larsc
resources/tools-software/linux-drivers/hwmon/ltc2947.txt · Last modified: 07 Jan 2020 13:50 by nsa