Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:tools-software:linux-drivers:drm:hdl-axi-hdmi [16 Feb 2015 11:12] – [Status] Lars-Peter Clausen | resources:tools-software:linux-drivers:drm:hdl-axi-hdmi [27 Jan 2021 22:35] (current) – use wp> interwiki links Robin Getz |
---|
| |
^ Source ^ Mainlined? ^ | ^ Source ^ Mainlined? ^ |
| [[linux.github>xcomm_zynq?drivers/gpu/drm/analog/analog_drm_drv.c|drivers/gpu/drm/analog/analog_drm_drv.c]] | [[git.linux.org>drivers/gpu/drm/analog/analog_drm_drv.c|WIP]] | | | [[linux.github>master?drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_drv.c|drivers/gpu/drm/analog/analog_drm_drv.c]] | [[git.linux.org>drivers/gpu/drm/adi/axi_hdmi_drv.c|WIP]] | |
| |
===== Files ===== | ===== Files ===== |
| |
^ Function ^ File ^ | ^ Function ^ File ^ |
| driver | [[linux.github>xcomm_zynq?drivers/gpu/drm/analog/analog_drm_drv.c|drivers/gpu/drm/analog/analog_drm_drv.c]] | | | driver | [[linux.github>master?drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_drv.c|drivers/gpu/drm/adi/axi_hdmi_drv.c]] | |
| driver | [[linux.github>xcomm_zynq?drivers/gpu/drm/analog/analog_drm_drv.h|drivers/gpu/drm/analog/analog_drm_drv.h]] | | | driver | [[linux.github>master?drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_drv.h|drivers/gpu/drm/adi/axi_hdmi_drv.h]] | |
| driver | [[linux.github>xcomm_zynq?drivers/gpu/drm/analog/analog_drm_crtc.c|drivers/gpu/drm/analog/analog_drm_crtc.c]] | | | driver | [[linux.github>master?drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_crtc.c|drivers/gpu/drm/adi/axi_hdmi_crtc.c]] | |
| driver | [[linux.github>xcomm_zynq?drivers/gpu/drm/analog/analog_drm_crtc.h|drivers/gpu/drm/analog/analog_drm_crtc.h]] | | | driver | [[linux.github>master?drivers/gpu/drm/adi_axi_hdmi/axi_hdmi_encoder.c|drivers/gpu/drm/adi/axi_hdmi_encoder.c]] | |
| driver | [[linux.github>xcomm_zynq?drivers/gpu/drm/analog/analog_drm_encoder.c|drivers/gpu/drm/analog/analog_drm_encoder.c]] | | |
| driver | [[linux.github>xcomm_zynq?drivers/gpu/drm/analog/analog_drm_encoder.h|drivers/gpu/drm/analog/analog_drm_encoder.h]] | | |
====== Example platform device initialization ====== | ====== Example platform device initialization ====== |
| |
===== Others ===== | ===== Others ===== |
| |
Since the driver registers a [[http://en.wikipedia.org/wiki/Linux_framebuffer|Linux framebuffer device]] it is possible to use any application or toolkit which has support for it to display graphics on the HDMI output. This for example includes [[http://directfb.org/|DirectFB]], [[http://www.mplayerhq.hu/|mplayer]] and [[http://www.libsdl.org/|SDL]]. | Since the driver registers a [[wp>Linux_framebuffer|Linux framebuffer device]] it is possible to use any application or toolkit which has support for it to display graphics on the HDMI output. This for example includes [[http://directfb.org/|DirectFB]], [[http://www.mplayerhq.hu/|mplayer]] and [[http://www.libsdl.org/|SDL]]. |
| |
====== More information ====== | ====== More information ====== |