This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-build:generic:zynqmp [26 Aug 2020 21:40] – [Running the script in one line [with defaults]] Travis Collins | resources:tools-software:linux-build:generic:zynqmp [03 Sep 2020 21:23] – [DisplayPort - no picture?] Robin Getz | ||
---|---|---|---|
Line 112: | Line 112: | ||
===== DisplayPort - no picture? ===== | ===== DisplayPort - no picture? ===== | ||
+ | |||
+ | The default configuration for most of the projects is to use the HDMI output, and that is what the configuration is set up for. | ||
+ | |||
+ | For DisplayPort projects, you may need to add a custom '' | ||
< | < | ||
Line 123: | Line 127: | ||
</ | </ | ||
+ | After following that, the board should be rebooted. |