This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:tools-software:linux-build:generic:zynq [30 Mar 2023 12:51] – Remove mentioning of SDK and add 2021_R1 release branch Iulia Moldovan | resources:tools-software:linux-build:generic:zynq [02 Feb 2024 16:08] (current) – update: master -> main Marcelo Schmitt | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== The script method ===== | ===== The script method ===== | ||
- | We provide [[https:// | + | We provide [[https:// |
The script takes up to 3 parameters, but if left blank, it uses defaults: | The script takes up to 3 parameters, but if left blank, it uses defaults: | ||
Line 18: | Line 18: | ||
==== Running the script in one line [with defaults] ==== | ==== Running the script in one line [with defaults] ==== | ||
< | < | ||
- | wget https:// | + | wget https:// |
</ | </ | ||