This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:linux-build:generic:zynq [04 Feb 2021 07:55] – [Setup cross compile environment variables] Michael Hennerich | resources:tools-software:linux-build:generic:zynq [09 Jun 2021 12:51] – Change source path Iulia Moldovan | ||
---|---|---|---|
Line 41: | Line 41: | ||
<note tip> | <note tip> | ||
- | If not otherwise required always use the latest release! | + | Use the latest release, if not required otherwise! |
</ | </ | ||
Line 57: | Line 57: | ||
< | < | ||
- | dave@hal9000: | + | dave@hal9000: |
- | Branch | + | Branch |
- | Switched to a new branch '2015_R2' | + | Switched to a new branch '2019_R2' |
</ | </ | ||
Line 81: | Line 81: | ||
| 2019_R2 | Vivado 2019.1 | | | 2019_R2 | Vivado 2019.1 | | ||
- | Vivado | + | Vivado |
< | < | ||
- | dave@hal9000: | + | dave@hal9000: |
</ | </ | ||
Line 90: | Line 90: | ||
< | < | ||
dave@hal9000: | dave@hal9000: | ||
- | dave@hal9000: | + | dave@hal9000: |
</ | </ | ||
+ | |||
+ | <note important> | ||
+ | Find the path to the Xilinx installation folder, and then use it to replace this string: **$PATH_to_Xilinx** that is written above. Same goes for the **$SDK_version**, | ||
+ | </ | ||
=== Using the Linaro toolchain === | === Using the Linaro toolchain === |