This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:linux-build:generic:raspberrypi [02 Nov 2020 23:54] – [Customizing the kernel/adding-drivers] Travis Collins | resources:tools-software:linux-build:generic:raspberrypi [08 Dec 2021 15:13] – add doc for Pi Zero Antoniu Miclaus | ||
---|---|---|---|
Line 49: | Line 49: | ||
ARCH=arm CROSS_COMPILE=< | ARCH=arm CROSS_COMPILE=< | ||
</ | </ | ||
+ | |||
+ | For Pi Zero, Pi Zero 2. | ||
+ | < | ||
+ | ARCH=arm make adi_bcmrpi_defconfig | ||
+ | ARCH=arm CROSS_COMPILE=< | ||
+ | </ | ||
+ | |||
===== Building the ADI kernel - script method ===== | ===== Building the ADI kernel - script method ===== | ||
Line 65: | Line 72: | ||
First backup the **kernel7.img** file on the SD-card. | First backup the **kernel7.img** file on the SD-card. | ||
- | The generated **arch/ | + | The generated **arch/ |
Any drivers built as modules must be installed onto the rootfs: | Any drivers built as modules must be installed onto the rootfs: |