This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:linux-build:generic:petalinux [16 Apr 2019 15:27] – [Building with Petalinx] Nuno Sá | resources:tools-software:linux-build:generic:petalinux [10 May 2019 16:16] – Nuno Sá | ||
---|---|---|---|
Line 31: | Line 31: | ||
{{ : | {{ : | ||
{{ : | {{ : | ||
+ | |||
+ | <note important> | ||
Depending on the platforms, a different device tree must be used. After finishing the previous steps, you must edit the **device-tree.bbappend** and set the **KERNEL_DTB** variable with the desired device tree. At the time of this writing these are the supported device trees: | Depending on the platforms, a different device tree must be used. After finishing the previous steps, you must edit the **device-tree.bbappend** and set the **KERNEL_DTB** variable with the desired device tree. At the time of this writing these are the supported device trees: |