This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:freertos:migration-guide:ucos-to-freertos-migration-guide [13 Jan 2020 03:24] – [Full API Map] sullivan liu | resources:tools-software:freertos:migration-guide:ucos-to-freertos-migration-guide [16 Jan 2020 09:40] – [Semaphores and Mutexes] Ann An | ||
---|---|---|---|
Line 312: | Line 312: | ||
**Example Usage** | **Example Usage** | ||
- | Here is a example in using the Queue Send from an interrupt in µC/ | + | Here is an example in using the Queue Send from an interrupt in µC/ |
<WRAP column 47%> | <WRAP column 47%> | ||
Line 373: | Line 373: | ||
**Deferred Interrupt Handling** | **Deferred Interrupt Handling** | ||
- | Both for µC/OS-III and FreeRTOS, it is normally | + | Generally, both for µC/OS-III and FreeRTOS, it is considered best practice to keep ISRs as short as possible. If there is a long-term response/ |
<WRAP column 30%> | <WRAP column 30%> | ||
Line 386: | Line 386: | ||
</ | </ | ||
- | The above diagram showing how is the deferred interrupt | + | The above diagram showing how the deferred interrupt |
</ | </ | ||
Line 1231: | Line 1231: | ||
<WRAP clear></ | <WRAP clear></ | ||
- | More examples in using the FreeRTOS Kernel Semaphores and Mutexes can be found in the FreeRTOS-Addin Examples. | + | More examples in using the FreeRTOS Kernel Semaphores and Mutexes can be found in the **[[resources/ |
+ | . | ||
---- | ---- | ||
Line 2198: | Line 2199: | ||
===== Further Reading ===== | ===== Further Reading ===== | ||
- | Further Reading | ||
To learn more about FreeRTOS including the API reference and the Features, Please refer to ADI FreeRTOS-Addin and FreeRTOS official web. | To learn more about FreeRTOS including the API reference and the Features, Please refer to ADI FreeRTOS-Addin and FreeRTOS official web. | ||