This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:crosscore:cces:quick-start [01 Oct 2020 17:11] – [CCES Setup - ICE-1000/ICE-2000 Emulator] Chad Wentworth | resources:tools-software:crosscore:cces:quick-start [01 Oct 2020 18:50] (current) – Chad Wentworth | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== CrossCore Embedded Studio(CCES) Quick Start for Windows ====== | ====== CrossCore Embedded Studio(CCES) Quick Start for Windows ====== | ||
- | This page is designed to allow users to quickly get connected to their Analog Devices evaluation boards using CCES. | + | This page is designed to show how to quickly get connected to Analog Devices evaluation boards using CCES. |
==== Hardware Connection Types ==== | ==== Hardware Connection Types ==== | ||
- | There are usually 2 ways that users can connect to evaluation boards. An In Circuit Emulator(ICE), | + | There are usually 2 ways to connect to ADI evaluation boards. An In Circuit Emulator(ICE), |
<WRAP round 70% tip> | <WRAP round 70% tip> | ||
- | For information on hardware connections | + | For information on hardware connections, how to to power up evaluation boards, or switch settings to allow for emulator/ |
</ | </ | ||
Line 51: | Line 51: | ||
=== Selecting the Application(s) to Load === | === Selecting the Application(s) to Load === | ||
{{: | {{: | ||
- | * In the **Name** edit box, users can select an appropriate name to describe the configuration, | + | * In the **Name** edit box, select an appropriate name to describe the configuration, |
* In the **Session** section, choose the program(s) to load (if the appropriate program is not already populated) when connecting to the board. | * In the **Session** section, choose the program(s) to load (if the appropriate program is not already populated) when connecting to the board. | ||
* If not loading any program upon connection to the target, do not make any changes. | * If not loading any program upon connection to the target, do not make any changes. | ||
Line 101: | Line 101: | ||
=== Selecting the Application(s) to Load === | === Selecting the Application(s) to Load === | ||
{{: | {{: | ||
- | * In the **Name** edit box, users can select an appropriate name to describe the configuration, | + | * In the **Name** edit box, select an appropriate name to describe the configuration, |
* In the **Session** section, choose the program(s) to load (if the appropriate program is not already populated) when connecting to the board. | * In the **Session** section, choose the program(s) to load (if the appropriate program is not already populated) when connecting to the board. | ||
* If not loading any program upon connection to the target, do not make any changes. | * If not loading any program upon connection to the target, do not make any changes. |