This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:crosscore:cces:getting-started:create [18 Jul 2018 21:49] – [Creating Projects in CCES] Andrew McLachlan | resources:tools-software:crosscore:cces:getting-started:create [07 Nov 2018 16:24] (current) – [Importing a Project] Chad Wentworth | ||
---|---|---|---|
Line 7: | Line 7: | ||
Each time you start CCES, you will be prompted for a workspace location. You can opt to default to a workspace directory by choosing to use a workspace directory as your default. You will not be prompted the next time you open CCES. | Each time you start CCES, you will be prompted for a workspace location. You can opt to default to a workspace directory by choosing to use a workspace directory as your default. You will not be prompted the next time you open CCES. | ||
- | {{ : | + | {{: |
Line 21: | Line 22: | ||
The **General Project Information** window will appear (Figure 2). This is where a name is given to the project being created. Then click **Next**. | The **General Project Information** window will appear (Figure 2). This is where a name is given to the project being created. Then click **Next**. | ||
- | |||
- | <note important> | ||
The next window is for **Processor Type**, which is where the processor being programmed is configured. Once the **Processor type** and its **Silicon revision** (branded on the processor package itself) have been set appropriately, | The next window is for **Processor Type**, which is where the processor being programmed is configured. Once the **Processor type** and its **Silicon revision** (branded on the processor package itself) have been set appropriately, | ||
Line 56: | Line 55: | ||
In the **Import Projects** window, click **Browse…** next to the **Select root directory** text box and navigate to the root folder of the project you want to import. Once the root is selected, any projects in that directory (or any sub-directory) will appear in the **Projects** box. Check the box for the project(s) you want to import. Then click **Finish**. | In the **Import Projects** window, click **Browse…** next to the **Select root directory** text box and navigate to the root folder of the project you want to import. Once the root is selected, any projects in that directory (or any sub-directory) will appear in the **Projects** box. Check the box for the project(s) you want to import. Then click **Finish**. | ||
- | <note important> | + | <note important> |
+ | ---- | ||
+ | {{navigation CCES Getting Started# |