This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:crosscore:cces:getting-started:create [24 Jul 2018 14:49] – [Importing a Project] Glen Anderson | resources:tools-software:crosscore:cces:getting-started:create [27 Sep 2018 17:46] – Chad Wentworth | ||
---|---|---|---|
Line 22: | Line 22: | ||
The **General Project Information** window will appear (Figure 2). This is where a name is given to the project being created. Then click **Next**. | The **General Project Information** window will appear (Figure 2). This is where a name is given to the project being created. Then click **Next**. | ||
- | |||
- | <note important> | ||
The next window is for **Processor Type**, which is where the processor being programmed is configured. Once the **Processor type** and its **Silicon revision** (branded on the processor package itself) have been set appropriately, | The next window is for **Processor Type**, which is where the processor being programmed is configured. Once the **Processor type** and its **Silicon revision** (branded on the processor package itself) have been set appropriately, |