This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:crosscore:cces:getting-started:create [18 Jul 2018 21:51] – [Workspace and Projects] Andrew McLachlan | resources:tools-software:crosscore:cces:getting-started:create [27 Sep 2018 17:46] – Chad Wentworth | ||
---|---|---|---|
Line 22: | Line 22: | ||
The **General Project Information** window will appear (Figure 2). This is where a name is given to the project being created. Then click **Next**. | The **General Project Information** window will appear (Figure 2). This is where a name is given to the project being created. Then click **Next**. | ||
- | |||
- | <note important> | ||
The next window is for **Processor Type**, which is where the processor being programmed is configured. Once the **Processor type** and its **Silicon revision** (branded on the processor package itself) have been set appropriately, | The next window is for **Processor Type**, which is where the processor being programmed is configured. Once the **Processor type** and its **Silicon revision** (branded on the processor package itself) have been set appropriately, | ||
Line 58: | Line 56: | ||
<note important> | <note important> | ||
+ | |||
+ | ---- | ||
+ | Next Topic: [[resources: | ||