Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:tools-software:crosscore:cces:getting-started:app [27 Aug 2019 16:16] – Steven MacDiarmid | resources:tools-software:crosscore:cces:getting-started:app [27 Aug 2019 16:54] (current) – Steven MacDiarmid |
---|
**-core** the core used to run the flash memory driver. | **-core** the core used to run the flash memory driver. |
| |
<note important>For heterogeneous processors containing ARM and SHARC+ cores, **core 1 must run the flash memory driver**.</note> | <note important>For processors containing ARM and SHARC+ cores, **core 1 must run the flash memory driver**.</note> |
| |
**-driver**: flash memory device driver (included with the Board Support Package installation) the processor uses to work with the board's flash device | **-driver**: flash memory device driver (included with the Board Support Package installation) the processor uses to work with the board's flash device |
| |
<code bash> | <code bash> |
cldp -proc ADSP-SC573 -emu ICE-1000 -core 1 -driver "<ADSP-SC5xx EZ-KIT BSP root directory>\ADSP-SC5xx_EZ-KIT\Examples\Device_Programmer\sc573\sharc\sc573_w25q128fv_dpia_Core1\sc573_w25q128fv_dpia_Core1.dxe" -core 1 -cmd prog -erase affected -file "<workspace directory>\Debug\CCES_Example_Core0.ldr" | cldp -proc ADSP-SC573 -emu ICE-2000 -core 1 -driver "<ADSP-SC5xx EZ-KIT BSP root directory>\ADSP-SC5xx_EZ-KIT\Examples\Device_Programmer\sc573\sharc\sc573_w25q128fv_dpia_Core1\sc573_w25q128fv_dpia_Core1.dxe" -core 1 -cmd prog -erase affected -file "<workspace directory>\Debug\CCES_Example_Core2.ldr" |
</code> | </code> |
| |
3. Under **Post-build steps**, populate **Command** field with appropriate command line (see //Figure 5//). | 3. Under **Post-build steps**, populate **Command** field with appropriate command line (see //Figure 5//). |
| |
<note warning>Do //not// copy and paste the command line from above as formatting differences will cause cldp.exe to fail.</note> | <note warning>Do //not// copy and paste the command line from above as formatting differences will cause cldp.exe to fail.</note> |
| |
{{:resources:tools-software:crosscore:cces:getting-started:08_postbuild_configuration.gif|}} | {{:resources:tools-software:crosscore:cces:getting-started:08_postbuild_configuration.gif|}} |