Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:tools-software:crosscore:cces:getting-started:app [27 Aug 2019 16:00] – Steven MacDiarmid | resources:tools-software:crosscore:cces:getting-started:app [27 Aug 2019 16:51] – Steven MacDiarmid |
---|
| |
=====Step 2: Write Application to Flash Memory===== | =====Step 2: Write Application to Flash Memory===== |
With the LDR file generated, the final step is to write your application to your device's SPI flash memory. This is handled via the Command Line Device Programmer (cldp.exe) utility. Again, we will use the [[blink example]] project created previously for the ADSP-SC573 EZ-KIT. | With the LDR file generated, the final step is to write your application to your device's SPI flash memory. This is handled via the Command Line Device Programmer (cldp.exe) utility. Again, we will use the [[resources:tools-software:crosscore:cces:getting-started:led-blink-app:sc573-blink|blink example]] project created previously for the ADSP-SC573 EZ-KIT. |
| |
Just as the JTAG interface does not directly access DDR memory when downloading the DXE during debug, the CLDP does not interact directly with the board's flash memory. Instead, it uses the processor to load a host driver to communicate with flash, then passes the LDR image via JTAG so the processor can write it by issuing the proper commands to the flash. To coordinate this, **cldp.exe** needs several command-line switches and arguments to initialize the JTAG programmer, load the flash driver to the processor, then load the LDR image to the EZ-Kit's memory, as follows: | Just as the JTAG interface does not directly access DDR memory when downloading the DXE during debug, the CLDP does not interact directly with the board's flash memory. Instead, it uses the processor to load a host driver to communicate with flash, then passes the LDR image via JTAG so the processor can write it by issuing the proper commands to the flash. To coordinate this, **cldp.exe** needs several command-line switches and arguments to initialize the JTAG programmer, load the flash driver to the processor, then load the LDR image to the EZ-Kit's memory, as follows: |
**-core** the core used to run the flash memory driver. | **-core** the core used to run the flash memory driver. |
| |
<note important>For heterogeneous processors containing ARM and SHARC+ cores, **core 1 must run the flash memory driver**.</note> | <note important>For processors containing ARM and SHARC+ cores, **core 1 must run the flash memory driver**.</note> |
| |
**-driver**: flash memory device driver (included with the Board Support Package installation) the processor uses to work with the board's flash device | **-driver**: flash memory device driver (included with the Board Support Package installation) the processor uses to work with the board's flash device |
3. Under **Post-build steps**, populate **Command** field with appropriate command line (see //Figure 5//). | 3. Under **Post-build steps**, populate **Command** field with appropriate command line (see //Figure 5//). |
| |
<note warning>Do //not// copy and paste the command line from above as formatting differences will cause cldp.exe to fail.</note> | <note warning>Do //not// copy and paste the command line from above as formatting differences will cause cldp.exe to fail.</note> |
| |
{{:resources:tools-software:crosscore:cces:getting-started:08_postbuild_configuration.gif|}} | {{:resources:tools-software:crosscore:cces:getting-started:08_postbuild_configuration.gif|}} |