This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools-software:bfin:adas1000 [12 Oct 2012 16:55] – cat Catherine Redmond | resources:tools-software:bfin:adas1000 [05 May 2016 18:26] (current) – Catherine Redmond | ||
---|---|---|---|
Line 19: | Line 19: | ||
This project demonstrates a framework developed for Visual DSP [[adi> | This project demonstrates a framework developed for Visual DSP [[adi> | ||
- | {{ : | + | {{ : |
- | ==== The software has been developed to ==== | + | === The software has been developed to === |
* Configure various registers of [[adi> | * Configure various registers of [[adi> | ||
* Read ECG or Test tone data from [[adi> | * Read ECG or Test tone data from [[adi> | ||
Line 28: | Line 28: | ||
* Display/ | * Display/ | ||
- | ===== Requirements: | + | ==== Requirements: |
* VisualDSP++ 5.0 Update 10 | * VisualDSP++ 5.0 Update 10 | ||
* [[adi> | * [[adi> | ||
- | * SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++), | + | * SDP-B Rev 1.3 (with Emulator to connect to VisualDSP++), |
- | * Breakout board for SDP-B (If Hardware DRDY is used) [[adi> | + | * Breakout board for SDP-B (If Hardware DRDY is used) |
* ECG cables and simulator (if required) | * ECG cables and simulator (if required) | ||
===== Framework Files ===== | ===== Framework Files ===== | ||
The attached zip file contains the relevant files for this project | The attached zip file contains the relevant files for this project | ||
- | {{:resources: | + | |
+ | |||
+ | Zip File Contents & description: | ||
* ADAS1000_SDP_v1.c Main function which can be used to develop the application | * ADAS1000_SDP_v1.c Main function which can be used to develop the application | ||
* ADAS1K_Functions.c All the functions related to ADAS1000, which can be used by the application to read/write ADAS1000 registers, | * ADAS1K_Functions.c All the functions related to ADAS1000, which can be used by the application to read/write ADAS1000 registers, | ||
Line 50: | Line 52: | ||
* SPORT_Functions.h - Declaration of all the SPORT1 functions used for Serial Interface with ADAS1000 | * SPORT_Functions.h - Declaration of all the SPORT1 functions used for Serial Interface with ADAS1000 | ||
* User_Config.h - All the user definable parameters for various functionalities of (ADAS1000 + SDP) system | * User_Config.h - All the user definable parameters for various functionalities of (ADAS1000 + SDP) system | ||
- | |||
* LA.vps - VDSP++ plot for LA data | * LA.vps - VDSP++ plot for LA data | ||
* LL.vps - VDSP++ plot for LL data | * LL.vps - VDSP++ plot for LL data | ||
Line 57: | Line 58: | ||
* V2.vps - VDSP++ plot for V2 data | * V2.vps - VDSP++ plot for V2 data | ||
- | + | ==== Implementation | |
- | ==== Implementation | + | |
* ' | * ' | ||
Line 70: | Line 70: | ||
- Process the captured frames | - Process the captured frames | ||
- Display the processed data | - Display the processed data | ||
- | |||
==== Procedure: ==== | ==== Procedure: ==== | ||
+ | === Hardware Setup === | ||
- | - | ||
- | - | ||
- | - | ||
Line 89: | Line 88: | ||
- Right click on the plot > Configure > Modify ' | - Right click on the plot > Configure > Modify ' | ||
- Halt the code, to see the latest ' | - Halt the code, to see the latest ' | ||
+ | ===== Zip file===== | ||
+ | {{: |