This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:tools-software:android-drivers:sensor-acceleration:adxl345 [09 Nov 2011 14:01] – Approved Michael Hennerich | resources:tools-software:android-drivers:sensor-acceleration:adxl345 [03 Jan 2013 20:42] – external edit | ||
---|---|---|---|
Line 98: | Line 98: | ||
</ | </ | ||
- | <note tip> | + | <WRAP tip> |
In case the ADXL345/6 is not always event0 you can alternatively approach via / | In case the ADXL345/6 is not always event0 you can alternatively approach via / | ||
- | </note> | + | </WRAP> |
* Rebuilt your Android tree | * Rebuilt your Android tree | ||
- | <note tip> | + | <WRAP tip> |
Upon start the Android log file (use logcat) should include following lines: | Upon start the Android log file (use logcat) should include following lines: | ||
Line 112: | Line 112: | ||
D/ | D/ | ||
</ | </ | ||
- | </note> | + | </WRAP> |
Line 122: | Line 122: | ||
The maximum sample rate is by default limited to 200Hz, to change this limit modify define ADXL_MAX_SAMPLE_RATE_VAL in the sensor file. | The maximum sample rate is by default limited to 200Hz, to change this limit modify define ADXL_MAX_SAMPLE_RATE_VAL in the sensor file. | ||
- | <note warning> | + | <WRAP alert> |
Very high sample rates > 400Hz can freeze your system! | Very high sample rates > 400Hz can freeze your system! | ||
- | </note> | + | </WRAP> |
<source master/ | <source master/ |