This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:ace [07 Mar 2018 19:57] – [ACE or SDP Driver Install Fails or Warns me the driver/exe is unsigned] Michael Fowler | resources:tools-software:ace [15 Mar 2018 00:06] – [ACE Does Not Discover High-Speed DAC Eval Boards] John Birnie | ||
---|---|---|---|
Line 49: | Line 49: | ||
The High-Speed DAC boards have a second on-board USB controller, make sure this is connected as well as the main FPGA controller board. To avoid potential confusion, ACE only reports boards on the second controller (where it is required). | The High-Speed DAC boards have a second on-board USB controller, make sure this is connected as well as the main FPGA controller board. To avoid potential confusion, ACE only reports boards on the second controller (where it is required). | ||
- | There is also a known driver conflict issue between the NI VISA driver and Keysight' | + | \\ |
+ | There is also a known driver conflict issue between the NI VISA driver and Keysight' | ||
+ | \\ | ||
+ | The same workaround may be necessary for Rhode-Schwarz VISA. | ||
+ | \\ | ||
If you need to automate equipment and use ACE at the same time you might have to use two separate PCs. The ACE remote control/ | If you need to automate equipment and use ACE at the same time you might have to use two separate PCs. The ACE remote control/ | ||
+ | \\ | ||
+ | Another possible issue causing ACE to not detect Hsdac boards is an outdated version of the " | ||
+ | |||
+ | This is the ACE log entry indicating an incompatible version of the " | ||
+ | Could not initialise DPG Client System.Exception: | ||
+ | System.Exception: | ||
+ | AnalogDevices.DPG.EvaluationBoards.Communication.DPG3_CSA.Finder.AttachedBoards(String[] DevicePaths) |