This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:ace [09 Oct 2017 13:07] – Ciaran Watterson | resources:tools-software:ace [07 Mar 2018 19:56] – Removed reference to Microsoft Root Certificate update as the files have been remoevd by Microsoft and ACE is signed such that the update is unnecessary anyway Michael Fowler | ||
---|---|---|---|
Line 23: | Line 23: | ||
- Make sure the PC is connected to the Internet and can get root certificate updates, normally this happens automatically. | - Make sure the PC is connected to the Internet and can get root certificate updates, normally this happens automatically. | ||
- | | + | |
- | - Make sure the setting below is either Not Configured or Disabled | + | - Make sure the setting below is either Not Configured or Disabled |
- | - {{ : | + | - {{ : |
- | - If you can't connect to the internet e.g. an "air gapped" | + | |
- | - See [[https:// | + | |
- Check for and install all the latest Windows updates | - Check for and install all the latest Windows updates | ||
- Check your group policy settings, these may be controlled by IT or a System Administrator | - Check your group policy settings, these may be controlled by IT or a System Administrator | ||
- | | + | |
- | - Run gpedit.msc and navigate to the setting below | + | - Run gpedit.msc and navigate to the setting below |
- | - {{ : | + | - {{ : |
Line 49: | Line 47: | ||
==== ACE Does Not Discover High-Speed DAC Eval Boards ==== | ==== ACE Does Not Discover High-Speed DAC Eval Boards ==== | ||
- | The High-Speed DAC boards have a second on-board USB controller, make sure this is connected as well as the main FPGA controller board. To avoid potential confusion ACE only reports boards on the second controller (where it is required). | + | The High-Speed DAC boards have a second on-board USB controller, make sure this is connected as well as the main FPGA controller board. To avoid potential confusion, ACE only reports boards on the second controller (where it is required). |
There is also a known driver conflict issue between the NI VISA driver and Keysight' | There is also a known driver conflict issue between the NI VISA driver and Keysight' |