This is an old revision of the document!
This is a landing page for up-to-date information and examples pertaining to the ACE remote control feature. This feature allows a user to control ACE and evaluation hardware from other languages/applications.
Currently 1GB of data can be captured with the ADS8V1 and 2GB of data can be captured with the ADS7V2 using the AsyncRawCaptureToFile transaction. The following example shows how this transaction can be used from a Python script with the AD9208 evaluation platform.
Setup: AD9208 board connected to ADS7V2 or ADS8V1 motherboard. ADC clock = 3GHz, REFCLK = 375 MHz
Python Code:
# Copyright (c) 2019 Analog Devices, Inc. All Rights Reserved. This software is proprietary to Analog Devices, Inc. and its licensors. # These code snippets are provided ‘as is’ with no warranties, guarantees of suitability, or acceptance of any liability, for their use. import clr import sys import os import time # Connect to ACE using the remote control client sys.path.append(r'C:\Program Files (x86)\Analog Devices\ACE\Client') clr.AddReference('AnalogDevices.Csa.Remoting.Clients') import AnalogDevices.Csa.Remoting.Clients as adrc clientManager = adrc.ClientManager.Create() client = clientManager.CreateRequestClient('localhost:2358') # Load the AD9208 plug-in client.AddHardwarePlugin('AD9208-3000EBZ') # Navigate to initialization wizard and set to one converter client.set_ContextPath(r'\System\Subsystem_1\AD9208-3000EBZ\AD9208') client.NavigateToPath('Root::System.Subsystem_1.AD9208-3000EBZ.AD9208') client.SetWizardParameter('initwizard','jtx_m_cfg','0') time.sleep(2) client.ApplyWizardSettings('initwizard','Apply') # Navigate to capture wizard and set the number of samples to 500MSamples (1GB) client.NavigateToPath('Root::System.Subsystem_1.AD9208-3000EBZ.AD9208.AD9208 Analysis') client.SetWizardParameter('captureWizard','validatedSampleCount',str(2**29)) # Divert the output of the ADS7V2/ADS8V1 to a file client.AsyncRawCaptureToFile(os.path.expanduser('~\Desktop\largeCapture.bin'),'test','false','true') # Wait up to 5secs for the capture to complete client.WaitOnRawCaptureToFile('5000','test','false',os.path.expanduser('~\Desktop\largeCapture.bin'))
Download Python and Jupyter Notebook versions of this example: large_capture_example.zip
More information on the following example will be added.