This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:ace:knownissues [27 Jul 2018 00:46] – provide link to DPGDownloader Michael Fowler | resources:tools-software:ace:knownissues [11 Mar 2019 21:45] – Added description of "Update Software Regsiters" option in the Register Debugger Matt McCarn | ||
---|---|---|---|
Line 35: | Line 35: | ||
===== Register Debugger Does Not Update Software Values ===== | ===== Register Debugger Does Not Update Software Values ===== | ||
- | While not a bug, the behavior of the register debugger can be confusing and lead users to think that ACE is not successful communicating to the hardware. The register debugger writes directly to the hardware, and it does not update register values stored in the software. This will cause the register map to be out of sync between the hardware and the software. The registers that are out of sync will be indicated by bold lettering in the register map, as seen in the figure below. If the user clicks the "Apply Changes" | + | While not a bug, the behavior of the register debugger can be confusing and lead users to think that ACE is not successful communicating to the hardware. The register debugger |
\\ | \\ | ||
+ | {{: | ||
- | {{ : | + | As of ACE 1.13, there is an option to change the behavior of the register debugger using the " |
- | + | ||
+ | {{: | ||
+ | |||
\\ | \\ | ||