This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:ace:knownissues [21 Aug 2019 12:46] – Ciaran Watterson | resources:tools-software:ace:knownissues [23 Aug 2019 17:55] – [High-Speed DAC Eval Boards are not discovered] Max Lehuraux | ||
---|---|---|---|
Line 13: | Line 13: | ||
- | ===== ACE Does Not Discover | + | ===== High-Speed DAC Eval Boards |
The High-Speed DAC boards have a second on-board USB controller, make sure this is connected as well as the main FPGA controller board. To avoid potential confusion, ACE only reports boards on the second controller (where it is required). | The High-Speed DAC boards have a second on-board USB controller, make sure this is connected as well as the main FPGA controller board. To avoid potential confusion, ACE only reports boards on the second controller (where it is required). | ||
\\ | \\ | ||
- | There is also a known driver conflict issue between the NI VISA driver and Keysight' | + | As of version 1.14, ACE replaces the driver of the on-board controller to avoid any of the conflicts with VISA drivers listed below and installs the DPGDownloaderLite application to replace the High-Speed DAC Software Suite. |
+ | |||
+ | However, at this time, some High-Speed DAC Eval Boards are not yet supported through ACE but through a dedicated SPI application that requires the NI VISA driver. | ||
+ | The recommended action if you are actively using these High-Speed DAC Eval Boards with dedicated SPI applications is to not update to ACE version 1.14 or install version 1.13 available [[http:// | ||
+ | |||
+ | \\ | ||
+ | For ACE version 1.13 and earlier, there is a known driver conflict issue between the NI VISA driver and Keysight' | ||
\\ | \\ | ||
The same workaround may be necessary for Rhode-Schwarz VISA. | The same workaround may be necessary for Rhode-Schwarz VISA. |